About CY7C65213

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
YoIs_1298666
Level 5
Level 5
250 sign-ins 100 replies posted 100 sign-ins

Hello,

I have three questions.

1. Can we enter suspend mode from CY7C65213?

    and if CY7C65213 is in suspend mode, which state is TXD pin(Hi-Z / High / Low(0V))?

2. Can we set TXD to Low(0V) ? for example, if we keep reset condition, can we set RXD to Low?

3. Can both D+ and D- be applied voltage without supplying voltage on VCC and VCCIO?

Best regards,

Yocchi

0 Likes
1 Solution
HirotakaT_91
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

Hello,

A1.

Yes, it supports suspend state as per the datasheet.

TxD pin will be Hi-Z mode in suspend state.

A2.

When reset is asserted to CY7C65213/CY7C65213A, all the I/O pins are tristated.

A3.

I am not expect such a situation.

Diagram of "Figure 2.  Self-Powered Configuration" in the datasheet is helpful if you would use RESET depends on VBUS status. During the device is reset, no current flows from the USBDP to USB host through a 1.5kohms pull-up resistor.

Best regards,

Hirotaka Takayama

View solution in original post

0 Likes
5 Replies
HirotakaT_91
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

Hello,

A1.

Yes, it supports suspend state as per the datasheet.

TxD pin will be Hi-Z mode in suspend state.

A2.

When reset is asserted to CY7C65213/CY7C65213A, all the I/O pins are tristated.

A3.

I am not expect such a situation.

Diagram of "Figure 2.  Self-Powered Configuration" in the datasheet is helpful if you would use RESET depends on VBUS status. During the device is reset, no current flows from the USBDP to USB host through a 1.5kohms pull-up resistor.

Best regards,

Hirotaka Takayama

0 Likes

Hello Takayama-san,

Thank you very much for your reply.

About A2. "tristated" means Hi-Z, right?

Best regards,

Yocchi

0 Likes

Hi,

Yes, that's right.

Best regards,

Hirotaka Takayama

0 Likes

Hello Takayama-san,

About A1, entering suspend mode is via USB control,

and the user cannot set or program this device into suspend mode,right?

Best regards,

Yocchi

0 Likes

Hi,

The user cannot set or program this device into suspend mode.

The device begins the transition to the Suspend state after the device sees a constant Idle state on its bus lines.

It is compliant with the USB spec.

Best regards,

Hirotaka Takayama

0 Likes