68013A Control Logic,Can ONLY Be Operated By FPGA? I want to use stm32 instead...

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi! I'm trying to use the slave FIFO function of the 68013A to transfer data via USB.

   

But I don't want to use FPGA because of some personal reason,

   

Can Stm32 do this job instead?

   

Looking forward to an instant reply ! 

   

Thank you !

0 Likes
1 Solution
Anonymous
Not applicable

 Hi,

   

      Yes, it's possible.If the IO standard of STM32 meets VOH, VOL, VIH and VIL specification of 68013A then it should work fine.

   

Thanks

   

Prajith

View solution in original post

0 Likes
2 Replies
Anonymous
Not applicable

 Hi,

   

      Yes, it's possible.If the IO standard of STM32 meets VOH, VOL, VIH and VIL specification of 68013A then it should work fine.

   

Thanks

   

Prajith

0 Likes
Anonymous
Not applicable

 Hi ainiludeer,

   

Not just FPGA or STM32 any processor for that matter should be able to interface with FX2LP.

   

Please check the timing parameters and if you'll be able to meet them, If not check the option of using STM32 as slave and FX2LP as the master of the interface using GPIF.

   

Regards,

   

Anand