cancel
Showing results for 
Search instead for 
Did you mean: 

USB Hosts Hubs Transceivers

Anonymous
Not applicable

 Hello friends, I need to create a USB OTG interface to make APPLE Iphone or IPAD USB OTG compatible to allow me to transfer Photos and documents between my Android Samsung Note Edge and my Iphone/ IPAD, OR is there any way to connect an External Flash Drive to APPLE Iphone or IPAD to allow bi directional transfer of Photos and documents between the Flash drive and the Iphone or IPAD or at least just being able to transfer PHOTOS from and Iphone or IPAD to the flash drive and from Flash drive to the Iphone/IPAD. Any suggestions or ideas?

   

Any HW and or SW solution to accomplish that? Does Cypress or other mfg have any IC that can help me accomplish the above Flash drive solution. Or is this just a SW solution or combination to save Photos and or documents from Iphone to flash drive and back to Iphone. Thanks Avi 

0 Likes
2 Replies
Anonymous
Not applicable

 Hi,

   

EZ host can act as host for more than one device.We have a RDk for this application(ez host acting as a host for mass storage devcies).

   

 

   

EZ host can act as host for full/high speed devices.It supports OTG functionality also.

   

 

   

If the apple phone can acts a OTG device you can consider EZ host for your application.But we haven't tested Apple phone with Ez-host.

   

 

   

But I don't think we can directly use Apple phones with other devices(not from Apple).

   

 

   

Regards,

   

Vikas.

0 Likes
Anonymous
Not applicable

 sorry forget to provide the links for datasheet and RDK

   

 

   

datasheet of Ez host :http://www.cypress.com/?id=187&rtID=107

   

Cy4640 RDk for mass storage application:http://www.cypress.com/?rID=14383

   

 

   

Regards,

   

Vikas.

0 Likes