cancel
Showing results for 
Search instead for 
Did you mean: 

USB Hosts Hubs Transceivers

GeFu_3059156
New Contributor

We are looking for lowest power USB hub with the following constraints:

1x high speed upstream port

1x high speed downstream port (removable)

1x full speed downstream port (non-removable)

We have looked at the datasheet for the CY7C65632/34 and see the following numbers

1 active high speed port = 51.9mA (typ) @ 3.3V = 171mW

Assume 85% efficient buck from 5V to 3.3  and power = 171/0.85 = 201mW

Is this power affected by transmission duty cycle?

We think we can save power by having external access to the core voltage. Is there a device like this????

By example a competitors device has dual supply inputs to separate internal LDOs

3.3V @ 25mA + 1.8V @ 24mA = 126mW

Again, assuming 85% efficient buck from 5V total power = 126/0.85 = 147mW

Does Cypress have something that will compete with this?

Geoffrey

0 Likes
1 Solution
Sananya_14
Moderator
Moderator

Hi Geoffrey,

HX2VL is our lowest power hub which we can recommend as per your requirements. Could you please explain what you are referring to as transmission duty cycle with respect to upstream USB bus?

We dont have separate access for the core voltage in HX2VL and the active power consumption ideally is as per your calculations. However, please check the suspend current which should be give a power consumption of 3.3V * 0.786 mA = 2.6 mW. Since idle state power consumption is an important parameter for most hub applications, please let us know if that can suit your requirement.

Best Regards,

Sananya

View solution in original post

0 Likes
3 Replies
Sananya_14
Moderator
Moderator

Hi Geoffrey,

HX2VL is our lowest power hub which we can recommend as per your requirements. Could you please explain what you are referring to as transmission duty cycle with respect to upstream USB bus?

We dont have separate access for the core voltage in HX2VL and the active power consumption ideally is as per your calculations. However, please check the suspend current which should be give a power consumption of 3.3V * 0.786 mA = 2.6 mW. Since idle state power consumption is an important parameter for most hub applications, please let us know if that can suit your requirement.

Best Regards,

Sananya

View solution in original post

0 Likes
GeFu_3059156
New Contributor

Thank you for your quick response.

In our case, operating power and not suspend power is our critical parameter. Our product which incorporates the hub needs to allow 8 hours of operation on a typical Android cellphone.

By transmission duty cycle, I mean the percent of time transmitting data. We transmit MJPEG video, a 4ms burst every 16ms.

I assume the power specified in the data sheet needs to be adjusted by the duty cycle to get average power. Is this true?

We will but an eval board of the HX2VL and run some tests. Thank you.

0 Likes
Sananya_14
Moderator
Moderator

Hello,

The operating power which we specify in the datasheet is actually measured on enumeration. So it does not take into account the transmission duty cycle but is the average power taken across three devices on attach only.

Please let us know if you have any queries while using the eval board.

Best Regards,

Sananya

0 Likes