Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
OlEr_1999891
Level 5
Level 5
50 replies posted 25 replies posted 25 sign-ins

Hi!

We are making special kind of HDMI-to-USB Type-C adapter where we intended to use CCG3 together with Parade PS8743. Since there is a built-in aux-mux in that mux, is there any need for us to route AIUX/SBU via the CCG3? We can apply AUX pull-up/down separately. We planned base the FW on the CYPD3125 Notebook code since we will design is rather similar to the EVK base-board design (external DP input, USB-C is DP source). Anything to consider in this combination?

Cheers

Olof

0 Likes
1 Solution

Hello,

The purpose of the crossbar in CCG3 is to detect for plug connection orientation and route the SBU lines to the AUX of Display depending on the connection. If this functionality can be met using the external Mux and if the respective pull ups can be added then you may route the SBU signals directly skipping the CCG3.

Best Regards,

Yatheesh

View solution in original post

0 Likes
3 Replies
YatheeshD_36
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello,

Please refer to the below reference design which uses CCG3 for HDMI to type C solution.

https://www.cypress.com/documentation/reference-designs/ez-pd-ccg3-based-hdmi-over-type-c-cable-refe...

Please note that we only provide the hardware schematic for the reference design, no firmware support is provided.

Best Regards,

Yatheesh

0 Likes

Hi!

We are actually making a HDMI-to-USB-C, not USB-C-to-HDMI as the reference is and for that (and to keep support for USB 3 / SS) we need to the alt-mode mux. So the design is rather similar to the CCG3 EVK. So question is if we need to use the AUX/SBU mux if we have the Parade mux in place.

Cheers

Olof

0 Likes

Hello,

The purpose of the crossbar in CCG3 is to detect for plug connection orientation and route the SBU lines to the AUX of Display depending on the connection. If this functionality can be met using the external Mux and if the respective pull ups can be added then you may route the SBU signals directly skipping the CCG3.

Best Regards,

Yatheesh

0 Likes