CYPD3175 FAILURES

Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
BiBr_4663101
Level 1
Level 1

We have had a couple of CYPD3175 IC's fail in a prototype dedicated charging port design using the direct feedback system. The most faults we've had is that the chips stop responding to a plug insertion. We verify that the internal core is running because we can measure 1.8V and the CC line is pulled up to +3.3V before insertion and drops to 1.7V or so during insertion. These are prototype boards that were working until this sudden fault. 

We've also had the controller IC suddenly start running very hot and fail after working with no problems for two weeks. We only noticed the failure because after a plug insertion the port turned on and off contiuously. We remove the cable and reinsterted it and the controller chip started to heat up and stop running.

We have studied the switch mode power supply for stability and the phase and gain margins are according to industry standards.

0 Likes
1 Reply
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi ,

1. May I know whether CCG3PA have been report any Fault? CCG3PA firmware have defined below faults, is the fault you are referring to?

    FAULT_TYPE_VBUS_OVP = 0,    /* 0 */

    FAULT_TYPE_VBUS_UVP,        /* 1 */

    FAULT_TYPE_VBUS_OCP,        /* 2 */

    FAULT_TYPE_VBUS_SCP,        /* 3 */

    FAULT_TYPE_CC_OVP,          /* 4 */

    FAULT_TYPE_VCONN_OCP,       /* 5 */

    FAULT_TYPE_SBU_OVP,         /* 6 */

    FAULT_TYPE_OTP,             /* 7 */

2. You have mentioned that the controller IC suddenly start running very hot, Is the power shorten?

3. Could you please kindly share VDDD, VCCD, VBUS_IN_DISCHARGE, CC waveform when the issue is occurred?

4. May I know the schematic of your project?

5. May I know which firmware project you are testing?

Best Regards,

Lisa

0 Likes