Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
I am trying to configure an Infineon Aurix TC334 Lite kit QSPI as master. So far, I managed to configure the necessary pins, change the polarity to work with Gyro 6 Click Gyroscope (bit order - MSB, sampling edge - riging). I using an SPI sniffler and as far as i can see data is being transmitted but i receive nothing on MISO. Do you have any idea?
I've attached a snip with the SPI MOSI/MISO and the code as well.
Show Less
Hello dear infineon frends,
I currently have a problem with the Tricore from Infineon. The controller is currently being used in series production. Some controllers do not start after a reset. When I connect to the debugger/JTAG and execute the debug software reset, the application starts normally. If I do a hardware reset, the controller hangs.
I have compared working controller with the faulty controller. Working controller starts after "Idle mode" → "Normal mode". Faulty controller starts after "Idle mode" → "Sleep mode". Can you perhaps give me a tip on what I should look for? What is the reason for this problem?
Many thanks in advance
Greetings
Alexander
Dear Mr\Mrs,
I tried to create a project starting of Modustoolbox for IAR embedded. Compiling is failing with this issue:
"Error[Li005]: no definition for "__iar_Initlocks" [referenced from C:\Users\emanuelebelpanno\mtw\Empty_PSoC4_App\Debug\Obj\TOOLCHAIN_IAR_13573725619442129044.dir\cy_clib_support_iar.o]"
I've tried to look for this function and it isn't present in the project. How Cam I solve this issue?
I'm using Windows 10, IAR embedded ARM 9.50.2.
Kind Regards,
EB
Show LessHello Infineon Community,
We are unable to identify the MAC-ID of Infineon Aurix Tc397xx having transceiver ID as RTL8211F with connected RJ45 cable controller to the Canoe for my project activities.
Please help in this regard how to connect the MAC-ID of the specific chi set to Canoe
Thanks in advance
Show LessHello, I would like to know what are TSN standards does the Aurix TC399 microcontroller supports?
In the end, the target array is still all zeros
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/cyt4fbb7-%E4%BD%BF%E7%94%A8mdma%E5%A4%8D%E5%88%B6%E6%95%B0%E7%BB%84%E6%B2%A1%E6%9C%89%E6%88%90%E5%8A%9F%E6%98%AF%E4%B8%BA%E4%BB%80%E4%B9%88/td-p/724114
Show LessHi all,
with this post I´d like to understand wether there is a suitable successor for the CYRF69103 chip which has become obsolete.
I´m interested in replacing this chip on one of my projects with a nearly similar one. I already came accross one which has the label CYRF6935. Would this be an option? How long will this one be available on the market?
Looking forwards for one reply.
Thanks in advance,
Martin
Show Less
Hi,
I am currently working on sending and receiving frames on the Aurix TC397, I managed to send BUT the interrupt for "transmissionCompletedEnabled" does not seem to work.
I have received the frame inside my RX FIFO0 but the interrupt RX does not work either.
And because I am not doing the interrupt I can't read what's inside my FIFO.
In my config, I have the right flag enable :
- "transmissionCompletedEnabled" for TX
- "rxFifo0NewMessageEnabled" for RX
There are indeed enabled I had checked them on the CPU registers.
Here is my interrupt config for TX :
g_mcmcan.canNodeConfig.interruptConfig.transmissionCompletedEnabled = TRUE;
g_mcmcan.canNodeConfig.interruptConfig.traco.priority = ISR_PRIORITY_CAN_TX;
g_mcmcan.canNodeConfig.interruptConfig.traco.interruptLine = IfxCan_InterruptLine_2;
g_mcmcan.canNodeConfig.interruptConfig.traco.typeOfService = IfxSrc_Tos_cpu0;
Here is my interrupt config for RX FIFO0 :
g_mcmcan.canNodeConfig.interruptConfig.rxFifo0NewMessageEnabled = TRUE;
g_mcmcan.canNodeConfig.interruptConfig.rxf0f.priority = ISR_PRIORITY_CAN_RX;
g_mcmcan.canNodeConfig.interruptConfig.rxf0f.interruptLine = IfxCan_InterruptLine_1;
g_mcmcan.canNodeConfig.interruptConfig.rxf0f.typeOfService = IfxSrc_Tos_cpu0;
I don't know where to look to find a solution to this problem.
Thanks,
Do I need to download special software to program the microcontroller XMC4400-F100K512 BA? Is DSP software programming code applicable?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/XMC/XMC4400-F100K512-BA/td-p/722645
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023