Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
I tried coneccting CySmart 1.3.0.8 and CY8CKIT-042-BLE-A using default settings.
Then, too many peer devices were listed in master tab.
Could I delete peer devices from list when I push [start scan]?
and is there a way to display only Cypress(Infineon) devices on master tab?
Or Could I serch and sort devices with device name?
best regards
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-4/CySmart-configuration/td-p/741035
Show LessHi, I am using TC 387. Is it possible to do multi tasking in this board?
Hi,
I want to know CYT2B75CAE this controller is supporting AUTOSAR, If yes where i will get those information,
when i browse i am not able to find the information
Show LessHi I need to fetch data from ethernet module in ethernet_input function. But it crashes if I try to fetch anything.
ethernet_input(struct pbuf *p, struct netif *netif)
Is there any way to get data from there? I need to make some CAN packet using those.
Show Less
Hi, over the past week I was trying to write the flash memory of my psoc 6 using System Calls, more specifically using the Write Row System Call.
Looking into the datasheet:
To write a row, the SRAM_SCATCH_ADDR should be written in the IPC_STRUCT and in that addres, there has to be essentially the OPCODE, followed by the integrity check, followed by the flash addr to write, followed by all the data to write in that row (SRAM_SCATCH_ADDR + 0x0C + n*0x04 = Data word n)
However, I think this is not correct, in the SRAM_SCATCH_ADDR + 0x0C, there should be the address of where the data to write is located, in the case of my psoc, it has to be a pointer to a 512 byte long array that contains the data to write in the row.
Hope this helps.
Link to datasheet: PSoC 6 MCU: CY8C61x4, CY8C62x4 Architecture Technical Reference Manual (TRM) PSoC 61, PSoC 62 MCU (infineon.com)
Link to example where I found the error: PSoC-6-MCU-Device-Related-Design/Memory/CE220120 - PSoC 6 MCU Blocking Mode Flash Write/CE220120_Blocking_Mode_Flash_Write.cydsn/main_cm4.c at master · Infineon/PSoC-6-MCU-Device-Related-Design · GitHub
I am running bldc motor with the help of hall sensor but not able to get full no load speed.This motor has 1000 rpm but getting only upto 3500 rpm.
I am using example code to drive this motor whether this code support 10000 rmp.
My motor is working at 48v,750 W.Could you help to resolve this problem
Show LessHello,
Now I can use one TIMER to set one time interval and trigger one event as shown in the picture below.
And project is also attached.
Is it possible that I only use one timer to trigger different event according to different time interval?
Thanks!
BR,
Lila
Show LessHi Sir,
想請問6EDL7141 OCP 與current amplifier 的位置關係
datasheet 的方塊圖OCP是在current amplifier之前
application note的方塊圖 OCP在current amplifier之後
請問何者是正確的呢?
謝謝!
Show Less
Dear Infineon support team,
Development environment
OS: Windows 10 pro
Compiler: ARMCC V5.06 update 6 (build 750)
Tool: Keil v5
Device: TLE9879QXA40
Board: Custom
Motor: IPM BLDC Delta connection
Power spec. : DC 12[V] 80[A]
With the off-state diagnosis function, I want to diagnose before starting the main statement, and after starting the main statement, I want to turn off the off-state diagnosis function and ignore DS-sts.
The user manual also states to disable DS-current and ignore the DS-sts flag.
However, it is not explained how to ignore DS-STS.
Because of DS-STS, the PWM_EN function continues to be automatically turned off.
How can I ignore DS-STS and make PWM_EN function work?
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023