Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
Hello,
I am curious to know does IAR IDE, programmer tools support in Linux(Debian)OS.
I know its not a right forum to ask here.
It would be really helpful to know this.
Thanks
Kiran
Show LessHi guys , I want to use freeRtos with psoc4 and my mcu is cy8c4248azi and I followed this guide : have a only one difference guide uses freeRtosV9.0.0 I used freeRTOSV202012.00
https://iotexpert.com/psoc4-freertos-port/
and I got this errors :
Do you have any idea what is the problem?
Show Less大家好 :
关于ADC和DMA 有几个疑问,想得到帮助。
1.官方例程TLE9879_DMA_ADC1中,adc_ch_result[DMA_CH0_NoOfTrans]数组设置为8,但是IFXCONFIG里面,图1所示序列模式勾选了14个(7个通道+7个通道4重复采集),那么这个地方,DMA在传数的时候,是不是把前几个就给覆盖了?
2.DMA配置里,ADC1->RES_OUT7.reg这个配置是干嘛用的?
3.DMA完成中断触发条件是什么,是完成一个通道还是完成整个一次多通道扫描?
4.采集的数为什么设置为32位的,ADC是12位的。
5.如果我想测量2通道的ADC的数,一个P2.4的电压+一个VDH的电压,循环扫描,实时更新,该怎么配置。
因为资料较少,看了半天文档也是不明所以,希望得到解答。
Show Less
For 1 to 1 trigger ,SAR ch is decided based on logical channel or ADC channel number?
Hi,
I was recently working with TC387.
I need to save some variables during standby mode, and after waking up, their value should not be initialized. I found the DLMU in the user manual, it is described as follows:
The data tested is defined in data section lmudata_cpu0, and the variable is successfully mapped.
Then before getting into standby mode, i changed the variable value to 0xAA.
At last, the standby mode gets into(the standby RAM is correctly selected).
But after waking up, the variable is still initialized with 0x55.
So could someone tell me why DLMU performs different from what the user manual has said, did i ignore something important?
Thanks!
Show Less大家好 请问有没有关于TLE9879的CSA例程,BLDC电机控制里想加一个电流检测,官方例程里没有关于CSA的例子,希望有使用过这个功能的分享一下经验。 谢谢!
If i purchase KIT_A2G_TC399_5V_TRB_S HW then
1) Will it have the Chip SAK-TC399XE-256F300S BD, mounted on it? OR
2) What chip (give me full name) , will be mounted in it so i can search its full capacity..?
Hello all,
I am able to see UCB_PLFASH register on my TC38x.
But UCB_DFLASH I am unable to see. Initially I was able to see and modify also with Trace32.
Can anyone suggest what to do?
PFA image for reference w.r.t current situation.
Thanks in advanced.
Show Less
请教, 我想参照参照XMC4400的PMSM_FOC_EXAMPLE_XMC44的Demo,用xmc4300实现PMSM_FOC_EXAMPLE_XMC44这个Demo。 现在遇到了我在选Queue C的时候没有这个选项,附件看图。请问怎么可以选到Queue C呢。xmc4300没有Queue C这个选项。
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023