Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
Does modustoolbox support CMSIS-DAP for debugging TRAVEO II, and if so, how do I set it up?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/modustoolbox-%E6%98%AF%E5%90%A6%E6%94%AF%E6%8C%81DAP/td-p/741605
Show LessWe use an Infineon FP 420 L 90 B magneto-resitive sensor to sense position in a precision tilt mechanism, but Infineon no longer makes this part. Does anyone know of a replacement part made by Infineon or another vendor that could take the place of this device?
Show Lesshi, Im music developer try to create new instrument basic on Eastern instrument ,i start my prototype with Arduino board .
I want to change for Infineon microprocessor ,I need same touchkeys function in this link .
- different dimensions keys board
- Bluetooth MIDI/OSC transmit messages controller
- 156 touch switch
- 26 touch keys with full midi/osc controller function
-OLED display
((My main question is which microprocessor i need to start with .))
Show Less
Hi, I am using Aurix TC375 Lite Kit development board and tried the freeRtos example code.
But after compilation, once the code is put in the debugger mode then the tsim issue comes as below snapshot --
Please get me a solution for this issue asap.
Thanks.
Show LessHi
I am wondering if you can attach the Eagle files for XMC_ECAT_PB-V2.1 or XMC_ECAT_PB-V3? I have asked this question previously but only received production files (see attached) not the raw .brd and .sch files. These help but I am looking to integrate the reference design into my own PCB and make changes to the layout. Thanks.
Show Less
Hello
My application calls the below function during a connection. It is configured as a peripheral. The connection interval is 100ms min/max with no 0 for slave latency. I'm reading a voltage from a sensor, sending it into an onboard opamp and then reading the output via the ADC. The problem is an inaccurate adc result. The reading I get is slightly higher by a few counts and sometimes toggles. If I don't call the function, the reading is accurate with no toggling.
I feel that placing the device into deepsleep between events is the issue but I don't know how to solve it. I've read the low power application note but I'm confused about what deepsleep does behind the scene. Do the GPIOs retain their states? Are the analog peripherals altered in any way? Is VREF affected?
thanks for your assistance.
void ManageLowPower(void)
{
CYBLE_LP_MODE_T bleMode;
uint8 interruptStatus;
if((CyBle_GetState() == CYBLE_STATE_ADVERTISING) ||
(CyBle_GetState() == CYBLE_STATE_CONNECTED))
{
/* Request BLE subsystem to enter into Deep-Sleep mode between connection and advertising intervals */
bleMode = CyBle_EnterLPM(CYBLE_BLESS_DEEPSLEEP);
/* Disable global interrupts */
interruptStatus = CyEnterCriticalSection();
/* When BLE subsystem has been put into Deep-Sleep mode */
if(bleMode == CYBLE_BLESS_DEEPSLEEP)
{
/* And it is still there or ECO is on */
if((CyBle_GetBleSsState() == CYBLE_BLESS_STATE_ECO_ON) ||
(CyBle_GetBleSsState() == CYBLE_BLESS_STATE_DEEPSLEEP))
{
/* Put the CPU into the Deep-Sleep mode */
CySysPmDeepSleep();
}
}
else /* When BLE subsystem has been put into Sleep mode or is active */
{
/* And hardware doesn't finish Tx/Rx opeation - put the CPU into Sleep mode */
if(CyBle_GetBleSsState() != CYBLE_BLESS_STATE_EVENT_CLOSE)
{
CySysPmSleep();
}
}
/* Enable global interrupt */
CyExitCriticalSection(interruptStatus);
}
}
Show Less
I am running bldc motor with the help of hall sensor but not able to get full no load speed.This motor has 1000 rpm but getting only upto 3500 rpm.
I am using example code to drive this motor whether this code support 10000 rmp.
My motor is working at 48v,750 W.Could you help to resolve this problem
Show LessHi I need to fetch data from ethernet module in ethernet_input function. But it crashes if I try to fetch anything.
ethernet_input(struct pbuf *p, struct netif *netif)
Is there any way to get data from there? I need to make some CAN packet using those.
Show Less
Hi, I can't add any printf or can't use UART from sample Ethernet application
if I add anything there it is crashing
I need to process data after receiving from Ethernet but if I try to do anything application just crash. So how and where to process Ethernet data.
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023