cancel
Showing results for 
Search instead for 
Did you mean: 

TRAVEO™ T2G

Sri_Cbe
New Contributor

Sri_Cbe_0-1632568891348.png

I am getting the error as in the image attached,using Miniprog4 for flashing(CYT2B98CA) it not sure why i am getting this error,It will be great if anyone can support to fix the error.

 

0 Likes
1 Reply
Ashish
Moderator
Moderator

Hi ,

Can you please attach the full log file (along with what command you are using to flash)? Also, are you using Cypress AutoFlash utility to program? Also it appears to be writing memory at SRAM reserved region at 0x08000000 which is not accessible to user code , so this may be cause of error, but please give the full log to understand issue better.

 

Regards,

Ashish

0 Likes