cancel
Showing results for 
Search instead for 
Did you mean: 

TRAVEO™ II

rloader
New Contributor II

Hi,

I can't see a statement of the valid temperature and voltages for the numbers on CYT3BB/4BB datasheet Table 26-7 "12-Bit SAR ADC DC Specifications". (Compare with the digital spec tables which have "–40 °C - 125 °C and for 2.7 V - 5.5 V except where noted").

The particular item of interest is the internal bandgap voltage (SID103A) - is the 2% accuracy at room temperature or over the full temperature range.

Cheers,
Ralph.

0 Likes
1 Solution
Pranith
Moderator
Moderator

Hello @rloader 

SID103A is valid for over the full temperature range. i.e, –40 °C <= TA <= 125 °C

Regards

View solution in original post

0 Likes
1 Reply
Pranith
Moderator
Moderator

Hello @rloader 

SID103A is valid for over the full temperature range. i.e, –40 °C <= TA <= 125 °C

Regards

View solution in original post

0 Likes