mesh realy feature

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
LeCa_2156671
Level 4
Level 4
First like received First like given

In wiced_bt_mesh_core_config_t  mesh_config, I can config features with/without WICED_BT_MESH_CORE_FEATURE_BIT_RELAY

to make device support/not support  relay feature.

But if I config support relay feature, relay feature is enabled when it's be provisioned.

Is there any place that I can modify to make relay feature is supported but disabled without config by Provisioner.

If all nodes's relay is enabled, I have to config it with "Config Relay Set" to disable the feature.

It's not convenient.

So is proxy feature.

0 Likes
1 Solution
Anonymous
Not applicable

Hi,

As per the present stack, the relay feature will be enabled during provision.

This has to be individually disabled. It cannot be left disabled during the provision.

View solution in original post

1 Reply
Anonymous
Not applicable

Hi,

As per the present stack, the relay feature will be enabled during provision.

This has to be individually disabled. It cannot be left disabled during the provision.