Studio Bluetooth

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
MaVo_3395126
Studio Bluetooth
I am using a CYW20706 based module (CYBT-343026).  I am using the modus toolbox example Audio_Sink for the CYW920706WCDEVAL platform.  The only change... Show More
MaVo_3395126
Studio Bluetooth
I have an A2DP device (cyw20706) that does not always reconnect to ios when disconnected.  Is there a way to attempt a reconnect from the device?   Show More
LiLe_3234306
Studio Bluetooth
Hi, I tried to test the LE OTA Apps for Android, which is in .\WICED-Studio-6.4\common\peer_apps\ota_firmware_upgrade\Android\LeOTAApp\app\build\outpu... Show More
Ezequiel
Studio Bluetooth
Hello! I'm using the CYBT-343026-01 module and I've been having problems with the  packetization modes of CYSPP. (I'm sending messages via BT and reci... Show More
hyhw_4628441
Studio Bluetooth
Hello,  i have found the sent HID data is repeated side on peer device when the HID connection is established.    SW Information - Chipset & EVK : CYW... Show More
wenchilo
Studio Bluetooth
malloc
Solved

Hi, I am working on CYBT-343026, but the firmware seems doesn't support malloc. Is there any API that can replace malloc?

TakMune
Studio Bluetooth
1. Does the I/F support master and slave mode?2. Is the frame mode supports short frames and long frames?3. Is the synchronization clock suppot 2.048M... Show More
TakMune
Studio Bluetooth

HFP codec of CYBT-3330xx-02 is PCM and CVSD?
Is there anything else?

jbiemar46456
Studio Bluetooth
Hello, I'm porting WICED to a STM32H733 and I've an issue with the code snip.bluetooth.ble_gatt_db.c. The function "wiced_bt_stack_init( ..);" is not ... Show More
YoJa_3107936
Studio Bluetooth
Hi Everyone It seems that the host side FW will need to be updated as the version of EZ-Serial changes in the End-Customer's environment.They would li... Show More