Studio Bluetooth Forum Discussions
Hi,
I'm testing chage mac address with Configuring the Bluetooth device address in CYW20706 link. I do the steps as below:
1. iBeacon-CYBT_343026_EVAL UART=COM31 downloadBT_DEVICE_ADDRESS=FFFFFFFFFFFF In the make target, then build.
2. send a HCI reset command (01 03 0C 00)---->response:04 0E 04 01 03 0C 00
3. send 01 10 FC 07 AA BB CC DD EE FF 00---->response:04 0E 04 01 10 FC 11
4. reset button press
I think there is once success with above steps. But today I tired again. Always fail. I don't know why. I use CYBT343026-01 EVAL board
BR,
Treacy
Show LessHi,
I'm custom a FW and I met a problem. If I use my custome FW to download to different devices, The mac address is same. How can I change the Mac address? Any document or examples advised to me? I use CYBT343026-01.(This is wiced_bt_dev_read_local_addr(bda); API, and this read address is same)
Show LessHi ,
I want to add OTA to watch demo in 20719(now in 20706) which communicate with host ST MCU through UART.
I have seen ota_firmware_upgrade demo and WICED-Firmware-Upgrade-Library.pdf,
but I have a question:
If I port those code to watch demo,should host ST do something with UART?
Thanks ,
Leo
Show LessHello,
I would like to implement the following BLE MIDI server with CYW20819.
CYW20819 needs to be developed with ModusToolbox, but the above sample is for WICED.
Can I import the BLE MIDI server library into ModusToolbox?
Best regards,
Kenji Takahashi
Show LessHello,
Is Module using CYW20820 released?
If there is a plan to release, please let me know the release date of ES and Production products.
Best regards,
Kenji Takahashi
Show LessHi All, DheerajP_41 AnjanaM_61
I have requirement like,
Board 1 is with mesh sensor server app, which publish data to mesh network.
Board 2 is with XXXXXX mesh application which subscribe the data from mesh network.
so if i send sensor data from Board1 , board2 should receive it.
i can do some workaround with existing light example and make it work, before putting hands i just want to know,
if any example code already exists ,which full fills for my requirement.
also i tried something in a short time.. which did not help..
In the Board2 i flashed mesh switch app, then below changes
wiced_bt_mesh_core_config_model_t mesh_element1_models[] =
{
WICED_BT_MESH_DEVICE,
// WICED_BT_MESH_MODEL_ONOFF_CLIENT,
WICED_BT_MESH_MODEL_SENSOR_CLIENT
};
// wiced_bt_mesh_model_onoff_client_init(ONOFF_SWITCH_ELEMENT_INDEX, NULL, is_provisioned);
wiced_bt_mesh_model_sensor_client_init(0, mesh_sensor_client_handler, is_provisioned);
my expectation was, to receive some events when Board1 publish data but did not happen,
let me know, if anyone can comment on this.
Thanks
Ashok
Show LessHi All, DheerajP_41
I enabled the debug option on project application setting and received following error. The board not detected , what could be the issue?
KIT : CYBT-213043-MESH EX_BT
my board detected as,
I installed jlink drivers ! but not compatible seems.
Thanks
Ashok r
Show Lessi'm looking for a Bluetooth Module.
CONDITIONS
・SPP required
・Version 4.2 or higher
・Smart Ready compatible (Classic +BLE)
・15mm×24mm×2.9mm or less
I found these as candidates.
・CYBT-423028-02
・CYBT-413034-02
However, I did not understand the specification of "WICED" in detail.
Do you have a detailed document on "WICED"?
I am waiting for an answer.
Show Less
Posting this for a customer as I believe this information would be useful to the community.
I’m a little confused about the capabilities of PCM interface from reading the CYW20706 datasheet. Is Time Division Multiplexing (TDM) supported on the PCM interface? Is it possible to specify the clock rate, frame sync rate, sample length, and slots used? For instance, in one application we might use 8 slots (channels), 32k samples per second, and 32-bit sample size. The resulting clock would be 8.192 Mhz (8 * 32 k * 32).
What are the capabilities, what are the limitations, what API's do I use to set up the interface, and where is this all documented?
Regards,
Corey
Show Less