cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

sagu_2642176
New Contributor

Hi all,

Before put bluetooth controller in Wake-on-BLE state, I need to filter advertisement packets with device address and some specific manufacturer data .

I used 0x05 LE_ADV_PCF (LE Adv Packet Content Filter) Feature Selection command but no success .

you can see in this example , I try to filter with XX XX XX XX XX XX address but command doesn't success (log with btmon)

< HCI Command: Vendor (0x3f|0x00e9) plen 14                                                                                                                                        #12 [hci0] 112.685279
    05 00 XX XX XX XX XX XX 00 20 00 00 00 00    ....m.... .... 
> HCI Event: Command Complete (0x0e) plen 5                                                                                                                                        #13 [hci0] 112.688789
  Vendor (0x3f|0x00e9) ncmd 1
    Status: Invalid HCI Command Parameters (0x12)
    05               

Have you any idea please?

0 Likes
1 Solution
MichaelF_56
Moderator
Moderator

The CYW20704 is not supported within the broad market and here on the IoT Community. You may want to reach out to your local Cypress sales/FAE team to line up factory support for this device.

View solution in original post

0 Likes
3 Replies
Anonymous
Not applicable

Which device are you using? Note that the command you are using is a vendor-specific command. So all devices might not support it.

0 Likes
sagu_2642176
New Contributor

I use 20704 device and this VSC command is supported by this device.

0 Likes
MichaelF_56
Moderator
Moderator

The CYW20704 is not supported within the broad market and here on the IoT Community. You may want to reach out to your local Cypress sales/FAE team to line up factory support for this device.

View solution in original post

0 Likes