cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

PeDo_4684411
New Contributor

This question is issued once again since the Developer Community has answer me to send a log file and then... nothing happened. The question was marked as solved but the system is still sending an error (communication with the module is OK but when reading the flash there is a mismatch). I am afraid that the module is not robust and mature enough and the investment done in producing and designing the cards is lost.

The last part of the log is shown here:

2020-11-18@11:22:34.983 Download config successfully had written 249 bytes to address 0xFF014343:  42 44 41 20 27 25 42 27 2C 20 43 6F 6E 6E 65 63 74 69 6F 6E 20 49 44 20 27 25 64 27 2C 20 52 65 61 73 6F 6E 20 27 25 64 27 0A 00 0A AC 00 F8 8E 21 00 00 00 00 C2 01 00 00 00 00 00 00 00 00 00 00 00 00 00 04 00 00 02 00 00 00 00 00 00 00 3D 7B 21 00 00 00 00 00 00 00 00 16 00 0A 00 0A 00 00 00 89 8F 21 00 18 00 02 00 02 00 00 00 87 8F 21 00 2A 00 04 00 04 00 00 00 EA 8F 21 00 2B 00 02 00 02 00 00 00 10 90 21 00 42 00 02 00 02 00 00 00 0E 90 21 00 43 00 07 00 07 00 00 00 80 8F 21 00 45 00 05 00 05 00 00 00 00 90 21 00 46 00 02 00 02 00 00 00 0C 90 21 00 06 00 00 27 01 00 00 40 03 50 72 6F 74 6F 4E 75 72 73 65 50 72 6F 74 6F 4E 75 72 73 65 00 3F FC 0A 7C 00 64 99 21 00 01 49 02 48 B8 F6 34 B8 79 7A 21 00 F8 AC 02 00 0B 48 0C 49 08 B5 88 42

2020-11-18@11:22:34.983 Sending bytes to HW:

114 bytes:  01 4C FC 6E 3C 44 01 FF 02 D0 0B 4A 18 F6 9C FA 0A 4A 00 21 0A 48 18 F6 9B FA FF F7 0C F8 09 4B ...

2020-11-18@11:22:34.998 Received bytes from HW:

7 bytes:  04 0E 04 01 4C FC 00

2020-11-18@11:22:34.998 Download config successfully had written 106 bytes to address 0xFF01443C:  02 D0 0B 4A 18 F6 9C FA 0A 4A 00 21 0A 48 18 F6 9B FA FF F7 0C F8 09 4B 09 4A 23 F0 0F 03 13 60 BD E8 08 40 00 F0 0E B8 F8 8E 21 00 F8 8E 21 00 A8 00 00 00 C4 09 00 00 A0 8F 21 00 64 9D 21 00 1C 24 20 00 4F F0 FF 31 08 B5 08 46 FF F7 1C F8 01 4B 02 4A 1A 60 08 BD 54 1D 20 00 39 7A 21 00 0B 04 00 75 99 21 00 FE 00 00

2020-11-18@11:22:34.998  Downloading config ...     (SOURCE:  CONFIG   Configuration data   build/ProtoNurse-CYBT_343026_EVAL-rom-ram-Wiced-release/ProtoNurse-CYBT_343026_EVAL-rom-ram-Wiced-release.hex)

2020-11-18@11:22:34.998 Sending bytes to HW:

9 bytes:  01 4D FC 05 00 00 00 FF 28

2020-11-18@11:22:35.013 Received bytes from HW:

47 bytes:  04 0E 2C 01 4D FC 00 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 66 ...

2020-11-18@11:22:35.013 ERROR: Download config error trying to verify 40 bytes at address 0xFF000000    (SOURCE:  CONFIG   Configuration data   build/ProtoNurse-CYBT_343026_EVAL-rom-ram-Wiced-release/ProtoNurse-CYBT_343026_EVAL-rom-ram-Wiced-release.hex) (Data mismatch at address 0xFF000000. Expected byte value 0x01 but device contains 0x66)

Thanks in advance. If the problem is related to the module I would like to know it as soon as possible to avoid the inversion to continue increassing.

0 Likes
1 Solution
SheetalJ
Moderator
Moderator

Hi PeDo_4684411​,

I have unmarked the uncorrect answer in thread- https://community.cypress.com/message/258789?et=watches.email.thread#258789 , the thread is open for discussion.

Also, from the logs you shared, I am not able to figure out exact problem. There should not be any problem while downloading through HCI using CYBT-343026-01 module. Please check your HCI UART pin connections once.

Can you once try programming the module using Chipload or Module Programmer to make sure if there is no problem with module?

View solution in original post

0 Likes
2 Replies
SheetalJ
Moderator
Moderator

Hi PeDo_4684411​,

I have unmarked the uncorrect answer in thread- https://community.cypress.com/message/258789?et=watches.email.thread#258789 , the thread is open for discussion.

Also, from the logs you shared, I am not able to figure out exact problem. There should not be any problem while downloading through HCI using CYBT-343026-01 module. Please check your HCI UART pin connections once.

Can you once try programming the module using Chipload or Module Programmer to make sure if there is no problem with module?

View solution in original post

0 Likes
AnjanaM_61
Moderator
Moderator

Hi PeDo_4684411 ,

Adding to SheetalJ_96 's response.

- I hope the error log which you provided is from download log of WICED Studio SDK . Am I correct?

- If then, is this happening with multiple modules or only for the same module / board?

- If you have not tried with multiple module/board, did you tried reprogramming the same module with another application and rechecked the download log ?

- After this download with error log, were you able to see the downloaded application running fine or do you see any issues ?

Can you please provide us some more details?

Thanks & Regards,

Anjana

0 Likes