cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

KeOn_
New Contributor II
I have a question about the CYBT-343026 module.
What is the maximum height of the CYBT-343026 module?
It is described on page 4 of the data sheet, but the calculation method is not clear.
0 Likes
1 Solution
HiNa_2357246
Contributor

Hi,

According to P4 of the data sheet, [Max Total module thickness] is calculated as follows.
0.5mm + 0.05mm + 1.45mm = 2.00mm

You can refer to the link below
https://community.cypress.com/message/211613?et=watches.email.thread#211613

View solution in original post

0 Likes
1 Reply
HiNa_2357246
Contributor

Hi,

According to P4 of the data sheet, [Max Total module thickness] is calculated as follows.
0.5mm + 0.05mm + 1.45mm = 2.00mm

You can refer to the link below
https://community.cypress.com/message/211613?et=watches.email.thread#211613

View solution in original post

0 Likes