Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Dear Forum,

I've found in datasheet that CYW20706 supports CTS wake up when talking about HCI UART

1. Low-power out-of-band BT_WAKE and HOST_WAKE signaling (datasheet section 1.1)

2. The CYW20706 UART can perform XON/XOFF flow control and includes hardware support for the Serial Line Input Protocol (SLIP).
It can also perform wake-on activity. For example, activity on the RX or CTS inputs can wake the chip from a sleep state
  (datasheet section 5.3)


Would you please tell how to implement the BT_WAKE or HOST_WAKE via UART?

Thanks!

Best Regards,

Tim Yu

0 Likes
1 Solution
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

There are dedicated pins to do BT_Wake (Pin F8) and BT_Host_Wake (F7) to realize these functions. For reasons that a pin can be multiplexed with other roles, make sure that they are explicitly selected for it in the applications.

View solution in original post

2 Replies
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

There are dedicated pins to do BT_Wake (Pin F8) and BT_Host_Wake (F7) to realize these functions. For reasons that a pin can be multiplexed with other roles, make sure that they are explicitly selected for it in the applications.

Anonymous
Not applicable

Thanks a lot!

I checked the latest datasheet. The CTS wake up description has been removed.

Best Regards,

Tim

0 Likes