cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

PeDo_4684411
New Contributor

I am using a RS232 FTDI adapter to download a hello_sensor_app through the HCI interface. The communication goes fine and the minidriver is launched OK but  the log file shows  the module memory has a mistmatch in the bytes writen and read.

I append here the last lines of the log:

A total of 2 contiguous memory areas were filled:

[FF000000..FF000027] DATA (40 bytes)

[FF003000..FF01419B] DATA (70044 bytes)

Download config error trying to verify 40 bytes at address 0xFF000000    (SOURCE:  CONFIG   Configuration data   build/hello_sensor-CYBT_343026_EVAL-rom-ram-Wiced-release/hello_sensor-CYBT_343026_EVAL-rom-ram-Wiced-release.hex) (Data mismatch at address 0xFF000000. Expected byte value 0x01 but device contains 0x66)

Please, help.

Thanks,

0 Likes
3 Replies
SheetalJ
Moderator
Moderator

Hi PeDo_4684411​,

Have you made any changes in .btp file or configuration files? Are you able to program the board using WICED IDE? Can you please attach full log of the error?

Make sure you have sent reset command initially and board is in download mode.

0 Likes
PeDo_4684411
New Contributor

Hi Sheetalj_96.

I have not made any change in those files you mentioned. I have follow the instructions  as indicated in KBA223428. The platform files used and modified as instructed in  KB221025. I am using the last  WICED Studio version available. I have no problems for initiating the downloading process as you can see in the log file attached after a Recovery Procedure.

Thank you in advance.

0 Likes
PeDo_4684411
New Contributor

Hi Sheetalj_96.

I have asked for a solution to a downloading problem related to a custom card that embed a CYBT-343026-01. The log file that demonstrates a good communication between the Wiced Studio and the module in the card have been sent without an answer. The log shows also that the problem occurs when reading the Flash. Can you help me or this is a failure associated to the module and the inversion I did to produce the cards is lost?

0 Likes