Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

NiLi_2861801
Level 3
First like received First like given
Level 3

Hi,

   I add sleep_configuration in sample mesh_battery_server.  I modified these codes:

1.  pin config:

wiced_platform_gpio_t platform_gpio_pins[]=

{

[PLATFORM_GPIO_0] = {WICED_P00, WICED_GPIO},

[PLATFORM_GPIO_1] = {WICED_P01, WICED_SPI_1_MISO},

[PLATFORM_GPIO_2] = {WICED_P07, WICED_SPI_1_CS},

[PLATFORM_GPIO_3] = {WICED_P17, WICED_GPIO},

[PLATFORM_GPIO_4] = {WICED_P25, WICED_I2C_1_SCL},

[PLATFORM_GPIO_5] = {WICED_P28, WICED_SPI_1_MOSI},

[PLATFORM_GPIO_6] = {WICED_P29, WICED_I2C_1_SDA},

[PLATFORM_GPIO_7] = {WICED_P33, WICED_UART_2_TXD},

[PLATFORM_GPIO_8] = {WICED_P34, WICED_UART_2_RXD},

[PLATFORM_GPIO_9] = {WICED_P38, WICED_SPI_1_CLK},

};

2. init flow

    g_sleepNow = WICED_FALSE;

    wiced_hal_i2c_init();

    wiced_hal_pspi_init(SPI1, SPI_MASTER, INPUT_PIN_PULL_UP, 0x00261C01, 1000000, SPI_MSB_FIRST, SPI_SS_ACTIVE_LOW, SPI_MODE_3, WICED_P07);

    wiced_result_t          result;

    wiced_sleep_config_t    sleep_config = { 0 };

    sleep_config.sleep_mode = WICED_SLEEP_MODE_NO_TRANSPORT;

    sleep_config.device_wake_mode = WICED_SLEEP_WAKE_ACTIVE_HIGH;

    sleep_config.device_wake_source = WICED_SLEEP_WAKE_SOURCE_GPIO;

    sleep_config.device_wake_gpio_num = WICED_P17;

    sleep_config.host_wake_mode = WICED_SLEEP_WAKE_ACTIVE_HIGH;

    sleep_config.sleep_permit_handler = battery_server_sleep_hanlder;

    result = wiced_sleep_configure(&sleep_config);

3.  sleep handler

static uint32_t battery_server_sleep_hanlder(wiced_sleep_poll_type_t type)

{

    uint32_t ret = WICED_SLEEP_NOT_ALLOWED;

    WICED_BT_TRACE(".");

    switch(type)

    {

        case WICED_SLEEP_POLL_SLEEP_PERMISSION:

            if( g_sleepNow == WICED_TRUE )

            {

                ret = WICED_SLEEP_ALLOWED_WITH_SHUTDOWN;

                WICED_BT_TRACE("$");

                //ret = WICED_SLEEP_ALLOWED_WITHOUT_SHUTDOWN;

            }

            break;

        case WICED_SLEEP_POLL_TIME_TO_SLEEP:

            if( g_sleepNow != WICED_TRUE )

            {

            ret = 0;

            }

            else

            {

                WICED_BT_TRACE("@");

            ret = WICED_SLEEP_MAX_TIME_TO_SLEEP;

            }

            break;

    }

    return ret;

}

4. button INT handler:

wiced_bool_t mesh_app_interrupt_handler(void* user_data, uint8_t pin)

{

  WICED_BT_TRACE("mesh_app_interrupt_handler\r\n");

  g_sleepNow = WICED_TRUE;

  wiced_bt_start_advertisements(BTM_BLE_ADVERT_OFF, 0, NULL);

  wiced_bt_ble_observe(WICED_FALSE, 0,NULL);

  wiced_bt_ble_scan(BTM_BLE_SCAN_TYPE_NONE, 0, NULL);

  return WICED_TRUE;

}

5. comments out the PERIODIC timer in mesh_application.c

When I push the USR BTN (P00), I saw the current lower down to nearly 400uA, the terminal ouputs the string which are in the function ->  battery_server_sleep_hanlder.

I attach a video named 1-activemode_to_sleep,mp4 ,

But , after a few minutes( 3 minutes or 7 minutes, 11 minutes, 20 minutes, I tried serveral times), The VBAT current will increase to 1.94mA, and the terminal will output nothing. Then I push the USR BTN again,  The board will reboot......

I also record a video named 2-dead_to_reboot,mp4. 

Another attacment file named QCOM_LOG.txt record the ouput strings.

what I described above will occur in other mesh samples.

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator First comment on KBA 5 questions asked First question asked
Moderator

Hi Nick,

Not sure you are working on this now.

1. a PERIODIC timer will prevent chip into SDS mode but only PDS mode, right?

A) Yes

2. It seems the mesh_samples will not enter SDS mode? (because I can see VBAT=0mA in other samples, but never saw 0mA in mesh samples. )

A) It should work. Have you tried it on latest WICED studio 6.2?

View solution in original post

0 Likes
6 Replies
NiLi_2861801
Level 3
First like received First like given
Level 3

Hi,

1. a PERIODIC timer will prevent chip into SDS mode but only PDS mode, right?

2. It seems the mesh_samples will not enter SDS mode? (because I can see VBAT=0mA in other samples, but never saw 0mA in mesh samples. )

3.

static uint32_t battery_server_sleep_hanlder(wiced_sleep_poll_type_t type)

{

    uint32_t ret = WICED_SLEEP_NOT_ALLOWED;

    WICED_BT_TRACE(".")

Why the red line will always output in the other samples , such asMotion Sensor Project with CYW20719/CYW20735​,  but not ouput in the mesh samples? 

And, after stopping scan&adv, it will be called!... ...

0 Likes
NiLi_2861801
Level 3
First like received First like given
Level 3

Hello,  any expert here can help me to resolve this problem?

Thanks very much!

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

Adding members of the applications engineering team who are familiar with Bluetooth Dual Mode and the CYW20719: madyyssuzhezzhxhyansanpmamkasirkranm

0 Likes
AnjanaM_61
Moderator
Moderator First comment on KBA 5 questions asked First question asked
Moderator

Hi Nick,

Not sure you are working on this now.

1. a PERIODIC timer will prevent chip into SDS mode but only PDS mode, right?

A) Yes

2. It seems the mesh_samples will not enter SDS mode? (because I can see VBAT=0mA in other samples, but never saw 0mA in mesh samples. )

A) It should work. Have you tried it on latest WICED studio 6.2?

0 Likes
NiLi_2861801
Level 3
First like received First like given
Level 3

Hi anpm,

    Thanks for your reply.  These problems have been replied in Mycases.  This thread can be closed, Thanks again.

0 Likes