cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

StN__1917156
Contributor

According to WBT101-03-RTOS ThreadX rtos is built into the device's ROM: How can use original ThreadX functions (not wiced_rtos...), which version of ThreadX is embedded into CYW20719 and which functions (if not all)? Any manuals, tutorials, examples?

Thanks

0 Likes
1 Solution
AbhishekK_31
Employee

The ThreadX version 5 (5.7) is used in the BT devices. We do not allow direct access to the ThreadX APIs. All RTOS related APIs can be found in wiced_rtos.h header file

View solution in original post

0 Likes
1 Reply
AbhishekK_31
Employee

The ThreadX version 5 (5.7) is used in the BT devices. We do not allow direct access to the ThreadX APIs. All RTOS related APIs can be found in wiced_rtos.h header file

View solution in original post

0 Likes