cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

MaMi_1707981
Contributor II

Can we use 3.073MHz as I2S clock for "48kHz, 16 bits, 2 channels" ?

The data rate is "48kHz, 16 bits, 2 channels -> 1.536 Mbps".

So, the clock rate is higher than the data rate.

Can CYBT343026 accept the settings ?

If yes, I think some padding data will be inserted in it.

Is the followings correct ?

    WS: 48kHz

    <Lch(16bit: MSB->LSB), padding(16bit)>,    <Rch(16bit, MSB->LSB), padding(16bit)>,    <Lch, padding>,    <Rch, padding>,  ...

0 Likes
1 Solution
SheetalJ
Moderator
Moderator

The only configuration we support is 16bit data with 32 Clocks. MSB Stuffing is not supported.

Please refer PCM/I2S Clock setting in CYW20706 for the allowed clock configuration.

View solution in original post

0 Likes
10 Replies
SheetalJ
Moderator
Moderator

I do not understand your query correctly. What do you mean by clock rate and data rate?

At I2S slave side, you don't have to set anything. WICED slave device will take care of the clock depending on the master clock. Just make sure that we support only 16 bit configuration.

0 Likes
MaMi_1707981
Contributor II

When A2DP data is "48 kHz, 16 bits, 2 channels", can we use 3.072MHz as I2S clock ?

0 Likes
SheetalJ
Moderator
Moderator

What do you mean by A2DP data is "48 kHz, 16 bits, 2 channels"? You mean 1.536 MHz clock?

0 Likes
MaMi_1707981
Contributor II

When A2DP Source data is 48kHz, 16 bits, 2 channels, then data rate is 1.536 bps.

In this case,

    Do we have to use just 1.536MHz as I2S clock ?

    Or, can we use any rate higher then 1.536MHz ?

0 Likes
SheetalJ
Moderator
Moderator

As given in PCM/I2S Clock setting in CYW20706 , WICED device I2S master only supports 1.536 MHz clock.

Whether as, if you are using some other I2S master (other than WICED device), then WICED device I2S slave rate can be upto 3.072 MHz, which is set by I2S master itself. You don't have to set the slave frequency separately; just configure the device as I2S slave.

MaMi_1707981
Contributor II

Hi SheetalJ_96,

As you wrote, I2S slave doesn't set clock rate.

So, if I2S master use 3.072MHz as I2S CLK, how does CYBT-343026-01 handle A2DP data which is encoded by 48 kHz 16 bits, 2 channels ?

Please find I2S_CLK3.072MHz_48kHz_16bit_2ch.png at response_#6 above.

0 Likes
MaMi_1707981
Contributor II

I'm sorry for rushing you, but It would be appreciate to reply soon.

0 Likes
SheetalJ
Moderator
Moderator

The only configuration we support is 16bit data with 32 Clocks. MSB Stuffing is not supported.

Please refer PCM/I2S Clock setting in CYW20706 for the allowed clock configuration.

View solution in original post

0 Likes
MaMi_1707981
Contributor II

In other words, does CYBT343026 support the signals with padding likes the attachment in I2S slave mode ?

0 Likes