Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
StN__1917156
Level 4
Level 4
25 replies posted 10 replies posted 5 replies posted

Keep getting those errors when connecting bonded Cysmart to CYW20719:

Status : Connection Terminated Due to MIC Failure (0x3d)

Encryption Status Event: bd ( 5a 10 0c ef 51 aa  ) res 8109

The CYW20719 hardware is CYBT_413034_EVAL.

Clients are Samsung TAB E 7” and Tab A 8” tablets with Android 4.4.4, 5.0.1 and 6.0.1

This error happens:

  1. Always if I pair let say Cysmart client1 on Android device 1 and disconnect, then pair another let say Cysmart client2 on Android device 2 and disconnect, RESET the CYW20719, then when return back to device1 and try to connect to CYW20719 (on Cysmart button on the right side shows ‘Paired’) so just click on the name of the CYW20719 a.k.a ‘Hello’ to reconnect and always (100%) will get ‘Connection Terminated Due to MIC Failure (0x3d)’.  So there is some logic to get error in this situation, because ‘hello_sensor’  code stores bonding info only for 1 bonding, but why this error will be MIC – isn’t MIC (message integrity check)  something similar to CRC?
  2. Random – this is the most annoying problem, because it happens when only one Device is bonded and  only this device trying to reconnect – sometimes connect, sometimes fail with the same MIC failure error (0x3d). And I tried plenty of different devices and Android OS versions: 4.4.4, 5.0.1, 6.0.1 and happened only with CYW20719.

So I already rise this problem couple months ago, but haven’t receive any solution (neither on any of the bugs I reported so far ☹ ), but at least:

Do you have some sniffer tool that could capture raw packets (incl. MIC) in the communication client <> server so to compare what is the difference when reconnecting go smooth and when fail?

Either there is something wrong on the Cypresses BT stack side or something in the timing parameters/syncs in the connection ☹   The only clue I could guess – slower processors with Android have more MIC failures than faster ones ☹ , but when I try reconnecting bonded CC2540 from TI, don’t have any problems neither with Cysmart, nor nRf Connect or other BLE Android clients on the same Android devices that fails with CYW20719 ☹

….

17:29:09.988 1 hello_sensor_management_cback: 17

17:29:09.992 1 Advertisement State Change: 0

17:29:09.992 1 ADV stop

17:29:09.994 RCVD [1] Event from HCI.  Name: HCI_Encryption_Change   (Hex Code: 0x08  Param Len: 4)

17:29:09.994                                   Status : Connection Terminated Due to MIC Failure (0x3d)

17:29:09.994                        Connection Handle : 64 (0x0040)

17:29:09.994                        Encryption Enable : 0 (0x00)

17:29:09.996 1 hello_sensor_management_cback: c

17:29:10.003 1 Encryption Status Event: bd ( 5a 10 0c ef 51 aa  ) res 8109

17:29:10.007 1 encryp change bd ( 5a 10 0c ef 51 aa  ) res: 8109

17:29:10.010 RCVD [1] Event from HCI.  Name: HCI_Disconnection_Complete   (Hex Code: 0x05  Param Len: 4)

17:29:10.010                                   Status : Success (0x00)

17:29:10.010                        Connection Handle : 64 (0x0040)

17:29:10.010                                   Reason : 61 (0x3d)

17:29:10.010 Connection Terminated Due to MIC Failure

17:29:10.014 1 connection_down 5a 10 0c ef 51 aa  conn_id:1 reason:61

0 Likes
5 Replies
SheetalJ
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 500 likes received

Hello StN._1917156​,

Please confirm if you are using WICED SDK 6.2.1? You can check /20719-B1_Bluetooth/wiced_tools/BTSpy for logs.

I will test your problem and update as soon as possible.

0 Likes

Hello,

Confirmed it is 6.2.1 (as already stated in the title) - 6.4 doesn't work at all with my hardware

The log that I've already posted is from BTSpy, but doesnt give me any clue except that the client (Android) terminated the connection because of MIC.

Now here is the same passage from the same test when it pass Ok:

17:31:40.884 RCVD [1] Event from HCI.  Name: HCI_Encryption_Change   (Hex Code: 0x08  Param Len: 4)

17:31:40.884                                   Status : Success (0x00)

17:31:40.884                        Connection Handle : 64 (0x0040)

17:31:40.884                        Encryption Enable : 1 (0x01)

17:31:40.889 1 hello_sensor_management_cback: c

17:31:40.893 1 Encryption Status Event: bd ( 5a 10 0c ef 51 aa  ) res 0

17:31:40.897 1 encryp change bd ( 5a 10 0c ef 51 aa  ) res: 0

0 Likes

Hi StN._1917156​,

I think you are referring toBug report – BLE – cant reconnect to a bonded device , we are not able to reproduce the issue.

Can you confirm if you have made any changes in the hello sensor demo app? Exact testing steps might help us to dig more.

0 Likes

Hi SheetalJ_96,

Yes, I'm referring to the same issue, but when I first reported it I was newbie with CYW, so there were and plenty bulk info that might cloud the core of the problem and it reproducing.

If you follow the situation #1 mentioned at the first post in this thread - I always receive this error with the original hello_sensor example from 6.2.1 (maybe only couple extra WICED_BT_TRACEs added and BT address fixed to never change).

So if you follow exactly scenario #1 from first post with Cysmart1.2 with default setting and hello_sensor example from WICED 6.2.1 - I always get those errors doesn't matter what android device and which version is.

Let me know if there is something I didn't explained clear enough how to reproduce the error and what are the prerequisites to start the experiment.

Thanks

EDIT: In described situation #1 in first post It is important to reset the board before return to reconnecting to not the last Cysmart client in order to reproduce 8109/61 error and then happens on 100% of all the devices and Android versions I tried so far

0 Likes
ZiSh_3434191
Level 3
Level 3
First solution authored 5 questions asked First like received

This error occurs when the resolving list has two entries for the same peer device.   Clearing the bonded list does not clear the resolving list. 

There are routines in the code example "BLE4.2_DataLength_Security_Privacy" to display the contents of the bonded list and resolving list.  Perhaps this will help identify what's going wrong.

0 Likes