cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

Leo_liu1
Contributor

Hi,

I am using CYW92070xV3_EVAL and WICED studio 6.1,my make target is "snip.mesh.mesh_onoff_server-CYW920706WCDEVAL LEGACY_BOARD=1 download"

But when i use app to add device ,can't scan my 20706.

my log as shown below:

setup nvram ids: net_key_max_num:4 app_key_max_num:8 3c-75

Mesh Start

[Rx]mesh_management_cback: 15

management_cback: LOCAL_IDENTITY_KEYS_REQUEST_EVT: result:0 keys:

mesh_management_cback: 0

***** Free mem before app_init:34684

## mesh_application_init ##

wiced_bt_[Rx]gatt_register: 0

ds1:0x00504000, len:0x0007e000

ds2:0x00582000, len:0x0007e000

platform btp: Config_DS_Location 0x00003000, Confi[Rx]g_VS_Location:0x00001000

WARNING: Upgrade will fail - active DS is not one of the expected locations

WARNING: Are ConfigDSLocation and DLConfigVSLocation in the .btp set up as in nv_loc_len[]?

mesh_application_init: wiced_bt_mesh_core_ota_fw_upgrade_init failed

[Rx]mesh_application_init: unprovisioned GATT DB status:0

***** Free mem after app_init:33156[Rx]

pastedImage_0.png

Thanks,

Leo

0 Likes
1 Solution
ShengY_96
Employee

Hi Leo

Per field debug, your phone can search the CYW20706's mesh device successfully.

And suggest to use the newer version of Wiced, like 6.2.1.

Regards

Jenson

View solution in original post

0 Likes
2 Replies
ShengY_96
Employee

Hi Leo

Suggest to use the CYW20735B1 and CYW20719B1 for mesh application.  And contact the local sales/FAE team for specified requirement.

Regards

Jenson

0 Likes
ShengY_96
Employee

Hi Leo

Per field debug, your phone can search the CYW20706's mesh device successfully.

And suggest to use the newer version of Wiced, like 6.2.1.

Regards

Jenson

View solution in original post

0 Likes