Smart Bluetooth Forum Discussions
HI everyone.
Board: BCM 20737 DK
SDK : 2.2.2 smart.
I want to do soft reset after button event. (To be more specific, I want to start the code from the beginning or power off my device)
However, I can not find any APIs for reset the firmware or power-off.
Is there any API call for reset, power-off, system-off or like these?
Thanks and have a good day
Regards, Jun-Kyu
Show LessHi, I have a question about option of make target.
I'd like to use both "download" and "download run" as make target option.
WICED Wi-Fi SDK supports these option. But WICED Smart SDK does not.
Is there any way to use both option on WICED Smart SDK?
SDK2.1.1 and later automatically starts the application after downloading.
And SDK 2.1.0 (or older), programmed application doesn't run by download.
Show LessHello everybody
I have wiced_sense tag when try to connect with my mobile phone it ask me form update to firmware1.3 and when I done the update from my mobile phone the wiced_sense work fine
But when I want to update to wiced sense from my SDK 2.1
Firstly when I build it make.file exe gives a eror . Then I changed the make file exe . I replace the make file exe in final1.3 firmware with the old firmware 1.1 then the build is done .
Application is running its ok.
But when I try to connect with my mobile phone again it ask me to update to 1.3 even I allready update it from my computer with SDK2.1
I have special extra codes inside the wiced_sense and for updating from my mobile phone ; Its not a good idea for protecting my extra codes.
What am I doing wrong ?
Show LessWICED Smart IDE - Eclipse IDE for C/C++ Developers 2.2.2
I'm running through the setup in WICED Smart Development Quick Guide
I've copied the hello_sensor and renamed to heart-monitor. When i double-click in "make target" i get this error.
I tried googling "eclipse perl.exe has stopped working" - no joy
Show LessDear All,
I want to implement Low power modes in BCM20737 BLE chip. Are there an API's available? I read in few documents about power modes in BCM chips and it says there are 2 power modes- Deep sleep mode and timed sleep mode. Is there any API's available to implement the same? Please suggest.
Reagards,
Prasanna
Show LessHi,
I am using accelerometer LIS3DH with BCM20737S and using WICED SDK 2.2.2 when I call library function "lis3dhInit" its showing following error on compilation.
C:\WICED\WICED-Smart-SDK-2.2.2\WICED-Smart-SDK\Wiced-Smart\spar/../../Apps/MyProject/MyProject.c:968: undefined reference to `lis3dhInit'
I have added the source and header file. Also it is invoking right function on F3 but not compiling it. Guidance is need what I'm missing or doing wrong.
Thanks in advance.
Kind Regard,
Ghalib
Show LessHi All,
We are using WICESDK for BCM20376, need to implement OS functionalities. Just wanted to clarify if the WICEDSDK supports OS concepts like creating thread,signals/events etc ? If so is there any documents bearing these?
Regards,
Prasanna
Show LessHello developers.
I'm programming these BCM20737S single chip modules with the WICED SMART IDE. My problem here is, why does two of the same kind of module act different, when i put the same software into them? (They are set to not to have same mac-address). I want the BLE modules to send data when connected to power (3.3V). One of them is sending the data continuously when connected to power through pin 3 (VBAT) 3,3V and a GND, while the other module is only sending once when connected. (Note that they both have the same software intergrated!) I have used the hello_sensor example. I have changed the BLE modules name and they both updated their names which can be seen through a BLE scanner which means that they both have downloaded the application.
One of the module are acting like it's suppose to do, while the other are doing some nonsense stuff.
Does anybody know why this is happening and what can i do?
Show Less===
SDK: 2.2.2
Tag: 920737.
app: hello-sensor based FW app.
OTA firmware size ~ 26KB.
===
Problem:
We find one problem that our device is using our app FW with version 1.2 and this
version is default bleprofile_Discoverable(NO_DISCOVERABLE, NULL)
by a mistake. However, our device is sealed with a SHELL outside PCB which
can not be downloaded by UART. So if we want to update this device with a
correct version(ADV available) by using OTA, it may not be connected with handset.
Is any possible way or back-door to let it feasible or possible?
For example, to let CPU pointer to elder version which is ok for ADV before to let
OTA available without destroying the device shell.
===
SDK: 2.2.2
Tag: 920737.
app: hello-sensor based app FW.
OTA firmware size ~ 26KB.
===
Problem:
we have a ADV LOCAL_NAME_LEN_MAX with "HELLO" and handset can scan it
but after we try to change it and make it longer as "HELLO SENSOR" in BLE_PROFILE_CFG,
handset can not find it as Unknown Device.
Do u know how to enlarge the NAME length and where to clean build the header file?
It seems the length is less than 17 char but handset can not find it.
Show Less