Smart Bluetooth Forum Discussions
why wiced sense does not work for iphone 4 even it is with iOS7.1?
Hi,
which SDK should I download for my WIndows XP?
Hi,
How can I control gpio pins in via supplied Android app?
thanks,
SJ
HW: BCM20736
SDK: 2.1.1
Question:
I use the BCM20736 as a central device, central need to discover all the servcies/characteristics/descriptors of the client.
As Core 4.1 spec-Vol3-PartG-Chapter4 said, use the Read-By-Group-Request to discover all primary/second services and all characteristics of special service, use the Find-Information-Request to discover all characteristic descriptors.
I can find the API "bleprofile_sendReadByGroupTypeReq" for Read-By-Group-Request, but I can't find the API for Find-Informaiton-Request, how to discover all characteristic descriptors?
Show LessHi everyone,
I am reaching out to the members of the forum to see if they recommend a EMI/EMC test and certification lab in San Francisco bay area.
We are a small startup working on a low budget and I am mostly looking for a quick and affordable EMI/EMC test and certification lab in San Francisco bay area which has prior experience in working with Broadcom Bluetooth SIP (BCM20732S).
Thanks,
Mehrdad
Show LessWhen I install WICED-Smart-SDK-2.1.1-IDE-Installer.exe
on my windows pc, I get a popup box with the message:
Error: Could not create the Java Virtual Machine.
Error: A fatal exception has occurred. Program will exit.
Anybody know what this means, and how to resolve?
-AC
Show LessI tried installing on Win 8.1 and getting the following error for Java runtime machine.
"Could not find a valid Java virtual machine to load
You may need to reinstall a supported Java virtual machine"
Which version of Java VM I need to install?
Thanks in advance.
Show Less
Hi,
we are going to choose seven Bluetooth USB dongles with the corresponding Bluetooth drivers in Windows for the following scenario:
we have a real master Bluetooth device and we want to connect up to seven Bluetooth devices(dongles attached to PC) at a time from the master device. All dongles could be from the same manufacturer. We write a Windows Bluetooth application to simulate the devices, so, we need also programmable API for drivers.
Now, for this scenario, is it possible to use only one driver( with programmable API or SDK) for those seven Bluetooth USB dongles simultaneously please?
Any note or hint is appreciated!
Thank you a lot!
Show Less
Hello,
I noticed that in the file ./Wiced-Smart/bsp/inc/20732mapa1.h, the naming convention for the defines is a bit clumsy.
Especially defining the word "version" line 225:
#define version (*(volatile unsigned int *)version_adr)
I had compiling issues because of using a structure member called "version".
This is not a bug but I just wanted to inform you of the possible issues it could lead to.
Thanks.
Show Less