Which 20737 pins can be configured as interrupts?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

   I looked through the BCM20737 datasheet and the BCM02737 Schematic Design Guidelines, but I didn't see this information. Where should I look?

0 Likes
1 Solution
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

There are up to 14 GPIOs on the module (40 on SOC)

  • Most can drive/sink up to 2mA
  • Capable of waking device from sleep or deep sleep
  • App can configure interrupts (both/either edges, level), pull-up/pull-down High-Z, etc.
  • Check theWICED™ Smart Hardware Interfaces to determine availability

View solution in original post

0 Likes
3 Replies
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

There are up to 14 GPIOs on the module (40 on SOC)

  • Most can drive/sink up to 2mA
  • Capable of waking device from sleep or deep sleep
  • App can configure interrupts (both/either edges, level), pull-up/pull-down High-Z, etc.
  • Check theWICED™ Smart Hardware Interfaces to determine availability
0 Likes
Anonymous
Not applicable

Thank you. I didn't know that any pin could be used as an interrupt; that is nice.

BTW, the 2mA drive current is kind of a pain; it forces one to use current buffers for simple LEDs. Most MCUs designed for ultra low power have a drive current of 4mA - 8mA.

0 Likes

dsmith

There's also 4 PWM channels on module (and SoC) and these can sink up to 16mA which make them ideal for controlling things like LEDs and Buzzers.

0 Likes