Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

  I have an application whereby we're using a BCM20737 in a remote control application to control multiple slaves at the same time. The application is controlling multiple lights at the same time from one pushbutton remote control. We're using a BCM20737 on the master and the slave. What is the maximum number of slaves that a BCM20737 master can control? Connection interval is approximately 500mSec, and data is very small; about 10B every 500mSec. Advertising interval on the slaves is 1000mSec.

Thanks,

Derek

0 Likes
1 Solution
Anonymous
Not applicable

Hello Derek,

I believe the BCM20737 configured as a Master can reliably connect to 7 devices depending on the use case.

Thanks

JT

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Hello Derek,

I believe the BCM20737 configured as a Master can reliably connect to 7 devices depending on the use case.

Thanks

JT

0 Likes