cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

SuLe_1710756
Contributor

Hi maxsong,

Our customer is considering to use serial flash to store user data. Could you confirm if customer is possible to use part number like attached files?

Thanks,

Sung-Mok

0 Likes
1 Solution
Anonymous
Not applicable

Hello Sung-Mok Lee,

Our SFLASH Drivers follow the command set of the Macronix Serial FLASH:

MX25U4033EM1I-12G.

From their manual:

http://www.macronix.com/Lists/DataSheet/Attachments/2641/MX25U4033E,%201.8V,%204Mb,%20v1.8.pdf

You have to make sure you can follow this command structure.

pastedImage_0.png

Thanks

JT

View solution in original post

0 Likes
3 Replies
Anonymous
Not applicable
0 Likes
MichaelF_56
Moderator
Moderator

sung-mok_lee

Per maxsong's request, I will ask the Applications team to check with the developers next week to determine if the MX25V1006E, 2.5V, 1Mb or EN25F10A-104XIP can be used as alternate NVRAM choices on your SoC design (on the SiP module, NVRAM in internal and cannot be modified).

More to follow next week.

lucyli j.t

0 Likes
Anonymous
Not applicable

Hello Sung-Mok Lee,

Our SFLASH Drivers follow the command set of the Macronix Serial FLASH:

MX25U4033EM1I-12G.

From their manual:

http://www.macronix.com/Lists/DataSheet/Attachments/2641/MX25U4033E,%201.8V,%204Mb,%20v1.8.pdf

You have to make sure you can follow this command structure.

pastedImage_0.png

Thanks

JT

View solution in original post

0 Likes