cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

Anonymous
Not applicable

Hi sir ,

Can tell me blecm_XXXXConMux methods meaning ?

111.jpg

Thanks Sir !

0 Likes
1 Solution
ArvindS_76
Employee

The next SDK release has these documented in the header. See hello_client for usage. In the meantime,

// The stack/app architecture supports only one connection at any point of time.

// Since the stack and app are event driven, a software mux is used to switch the

// app and stack connection context when some event/action needs to be performed on

// different connections. These functions provide the means to switch between different

// connection contexts.

// Internal function used by the stack to check if the connection context needs to be changed.

INT32  blecm_needToConMux( void );

/**

* Enable connection muxing. This needs to be done once by the app in the create function.

*/

void   blecm_enableConMux( void );

/**

* Disable connection muxing. Generally never done.

*/

void   blecm_disableConMux( void );

/**

* Initialize connection mux. This nees to be done once by the app in the create function.

* \param con_num The max number of connections that can be active at any point in time.

*/

void   blecm_ConMuxInit(INT32 con_num);

/**

* Add the connection to the list of known connections we can mux between. Typically done on connection up.

* \param index The index into which to add the connection information.

* \param con_handle The connection handle of this connection. This handle

*                    is used to look up the connection info structure.

* \param db_size  The size of the GATT DB to be associated with the connection.

* \param p_db The pointer to the GATT DB to be associated with this connection.

* \param dev_pinfo Device information in EMCONINFO_DEVINFO for this connection.

* \param smp_pinfo The SMP information from LESMP_INFO for this connection.

*/

void   blecm_AddConMux(INT32 index, UINT16 con_handle, UINT16 db_size, void *p_db,

                    void *dev_pinfo, void *smp_pinfo);

/**

* Delete the connection mux/context at the given index. Typically done on connection down.

* \param index The index of the connection information to delete.

*/

void   blecm_DelConMux(int index);

/**

* Find a free connection mux/context slot.

* \return Index of the first unused connection info structure or -1 when none are free.

*/

INT32  blecm_FindFreeConMux(void);

/**

* Look up the connection information structure given a handle.

* \param con_handle Connection handle of the connection to look up for.

* \return Index of the connection info structure or -1 when not found.

*/

INT32  blecm_FindConMux(UINT16 con_handle);

/**

* Get the GATT DB size given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return GATT DB size or 0 when not found.

*/

UINT16 blecm_GetDbSizeConMux(UINT16 con_handle);

/**

* Get the GATT DB  given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return GATT DB or NULL when not found.

*/

void   *blecm_GetDbConMux(UINT16 con_handle);

/**

* Get the device information given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return Device information pointer or NULL when not found.

*/

void   *blecm_GetDevConMux(UINT16 con_handle);

/**

* Get the SMP information given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return SMP information pointer or NULL when not found.

*/

void   *blecm_GetSmpConMux(UINT16 con_handle);

/**

* Reset the connection context.

*/

void   blecm_ResetPtrConMux(void);

/**

* Set all the connection contexts to the one for the given connection.

* This is used by the stack to switch connection contexts.

*/

void   blecm_SetPtrConMux(UINT16 con_handle);

// Internal function to check if 8-bitor 16-bit length is used in the app's GATT DB.

INT32  blecm_needToGATTDB16( void );

/**

* Enable 16-bit length fields in application GATT DB. This needs to be invoked before the first

* access to GATT DB occurs (early in create function). The GATT DB provided in the set_cfg function

* should use 16-bit lengths.

*/

void   blecm_enableGATTDB16( void );

/**

* Disable 16-bit length fields in app GATT DB.

*/

void   blecm_disableGATTDB16( void );

View solution in original post

2 Replies
MichaelF_56
Moderator
Moderator

Do you mean how these functions are used?  What they are used for, etc.?

What are you trying to use them for?

0 Likes
ArvindS_76
Employee

The next SDK release has these documented in the header. See hello_client for usage. In the meantime,

// The stack/app architecture supports only one connection at any point of time.

// Since the stack and app are event driven, a software mux is used to switch the

// app and stack connection context when some event/action needs to be performed on

// different connections. These functions provide the means to switch between different

// connection contexts.

// Internal function used by the stack to check if the connection context needs to be changed.

INT32  blecm_needToConMux( void );

/**

* Enable connection muxing. This needs to be done once by the app in the create function.

*/

void   blecm_enableConMux( void );

/**

* Disable connection muxing. Generally never done.

*/

void   blecm_disableConMux( void );

/**

* Initialize connection mux. This nees to be done once by the app in the create function.

* \param con_num The max number of connections that can be active at any point in time.

*/

void   blecm_ConMuxInit(INT32 con_num);

/**

* Add the connection to the list of known connections we can mux between. Typically done on connection up.

* \param index The index into which to add the connection information.

* \param con_handle The connection handle of this connection. This handle

*                    is used to look up the connection info structure.

* \param db_size  The size of the GATT DB to be associated with the connection.

* \param p_db The pointer to the GATT DB to be associated with this connection.

* \param dev_pinfo Device information in EMCONINFO_DEVINFO for this connection.

* \param smp_pinfo The SMP information from LESMP_INFO for this connection.

*/

void   blecm_AddConMux(INT32 index, UINT16 con_handle, UINT16 db_size, void *p_db,

                    void *dev_pinfo, void *smp_pinfo);

/**

* Delete the connection mux/context at the given index. Typically done on connection down.

* \param index The index of the connection information to delete.

*/

void   blecm_DelConMux(int index);

/**

* Find a free connection mux/context slot.

* \return Index of the first unused connection info structure or -1 when none are free.

*/

INT32  blecm_FindFreeConMux(void);

/**

* Look up the connection information structure given a handle.

* \param con_handle Connection handle of the connection to look up for.

* \return Index of the connection info structure or -1 when not found.

*/

INT32  blecm_FindConMux(UINT16 con_handle);

/**

* Get the GATT DB size given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return GATT DB size or 0 when not found.

*/

UINT16 blecm_GetDbSizeConMux(UINT16 con_handle);

/**

* Get the GATT DB  given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return GATT DB or NULL when not found.

*/

void   *blecm_GetDbConMux(UINT16 con_handle);

/**

* Get the device information given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return Device information pointer or NULL when not found.

*/

void   *blecm_GetDevConMux(UINT16 con_handle);

/**

* Get the SMP information given a connection handle.

* \param con_handle Connection handle of the connection to look up for.

* \return SMP information pointer or NULL when not found.

*/

void   *blecm_GetSmpConMux(UINT16 con_handle);

/**

* Reset the connection context.

*/

void   blecm_ResetPtrConMux(void);

/**

* Set all the connection contexts to the one for the given connection.

* This is used by the stack to switch connection contexts.

*/

void   blecm_SetPtrConMux(UINT16 con_handle);

// Internal function to check if 8-bitor 16-bit length is used in the app's GATT DB.

INT32  blecm_needToGATTDB16( void );

/**

* Enable 16-bit length fields in application GATT DB. This needs to be invoked before the first

* access to GATT DB occurs (early in create function). The GATT DB provided in the set_cfg function

* should use 16-bit lengths.

*/

void   blecm_enableGATTDB16( void );

/**

* Disable 16-bit length fields in app GATT DB.

*/

void   blecm_disableGATTDB16( void );

View solution in original post