The next SDK release has these documented in the header. See hello_client for usage. In the meantime,
// The stack/app architecture supports only one connection at any point of time.
// Since the stack and app are event driven, a software mux is used to switch the
// app and stack connection context when some event/action needs to be performed on
// different connections. These functions provide the means to switch between different
// connection contexts.
// Internal function used by the stack to check if the connection context needs to be changed.
INT32 blecm_needToConMux( void );
/**
* Enable connection muxing. This needs to be done once by the app in the create function.
*/
void blecm_enableConMux( void );
/**
* Disable connection muxing. Generally never done.
*/
void blecm_disableConMux( void );
/**
* Initialize connection mux. This nees to be done once by the app in the create function.
* \param con_num The max number of connections that can be active at any point in time.
*/
void blecm_ConMuxInit(INT32 con_num);
/**
* Add the connection to the list of known connections we can mux between. Typically done on connection up.
* \param index The index into which to add the connection information.
* \param con_handle The connection handle of this connection. This handle
* is used to look up the connection info structure.
* \param db_size The size of the GATT DB to be associated with the connection.
* \param p_db The pointer to the GATT DB to be associated with this connection.
* \param dev_pinfo Device information in EMCONINFO_DEVINFO for this connection.
* \param smp_pinfo The SMP information from LESMP_INFO for this connection.
*/
void blecm_AddConMux(INT32 index, UINT16 con_handle, UINT16 db_size, void *p_db,
void *dev_pinfo, void *smp_pinfo);
/**
* Delete the connection mux/context at the given index. Typically done on connection down.
* \param index The index of the connection information to delete.
*/
void blecm_DelConMux(int index);
/**
* Find a free connection mux/context slot.
* \return Index of the first unused connection info structure or -1 when none are free.
*/
INT32 blecm_FindFreeConMux(void);
/**
* Look up the connection information structure given a handle.
* \param con_handle Connection handle of the connection to look up for.
* \return Index of the connection info structure or -1 when not found.
*/
INT32 blecm_FindConMux(UINT16 con_handle);
/**
* Get the GATT DB size given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return GATT DB size or 0 when not found.
*/
UINT16 blecm_GetDbSizeConMux(UINT16 con_handle);
/**
* Get the GATT DB given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return GATT DB or NULL when not found.
*/
void *blecm_GetDbConMux(UINT16 con_handle);
/**
* Get the device information given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return Device information pointer or NULL when not found.
*/
void *blecm_GetDevConMux(UINT16 con_handle);
/**
* Get the SMP information given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return SMP information pointer or NULL when not found.
*/
void *blecm_GetSmpConMux(UINT16 con_handle);
/**
* Reset the connection context.
*/
void blecm_ResetPtrConMux(void);
/**
* Set all the connection contexts to the one for the given connection.
* This is used by the stack to switch connection contexts.
*/
void blecm_SetPtrConMux(UINT16 con_handle);
// Internal function to check if 8-bitor 16-bit length is used in the app's GATT DB.
INT32 blecm_needToGATTDB16( void );
/**
* Enable 16-bit length fields in application GATT DB. This needs to be invoked before the first
* access to GATT DB occurs (early in create function). The GATT DB provided in the set_cfg function
* should use 16-bit lengths.
*/
void blecm_enableGATTDB16( void );
/**
* Disable 16-bit length fields in app GATT DB.
*/
void blecm_disableGATTDB16( void );
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Do you mean how these functions are used? What they are used for, etc.?
What are you trying to use them for?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The next SDK release has these documented in the header. See hello_client for usage. In the meantime,
// The stack/app architecture supports only one connection at any point of time.
// Since the stack and app are event driven, a software mux is used to switch the
// app and stack connection context when some event/action needs to be performed on
// different connections. These functions provide the means to switch between different
// connection contexts.
// Internal function used by the stack to check if the connection context needs to be changed.
INT32 blecm_needToConMux( void );
/**
* Enable connection muxing. This needs to be done once by the app in the create function.
*/
void blecm_enableConMux( void );
/**
* Disable connection muxing. Generally never done.
*/
void blecm_disableConMux( void );
/**
* Initialize connection mux. This nees to be done once by the app in the create function.
* \param con_num The max number of connections that can be active at any point in time.
*/
void blecm_ConMuxInit(INT32 con_num);
/**
* Add the connection to the list of known connections we can mux between. Typically done on connection up.
* \param index The index into which to add the connection information.
* \param con_handle The connection handle of this connection. This handle
* is used to look up the connection info structure.
* \param db_size The size of the GATT DB to be associated with the connection.
* \param p_db The pointer to the GATT DB to be associated with this connection.
* \param dev_pinfo Device information in EMCONINFO_DEVINFO for this connection.
* \param smp_pinfo The SMP information from LESMP_INFO for this connection.
*/
void blecm_AddConMux(INT32 index, UINT16 con_handle, UINT16 db_size, void *p_db,
void *dev_pinfo, void *smp_pinfo);
/**
* Delete the connection mux/context at the given index. Typically done on connection down.
* \param index The index of the connection information to delete.
*/
void blecm_DelConMux(int index);
/**
* Find a free connection mux/context slot.
* \return Index of the first unused connection info structure or -1 when none are free.
*/
INT32 blecm_FindFreeConMux(void);
/**
* Look up the connection information structure given a handle.
* \param con_handle Connection handle of the connection to look up for.
* \return Index of the connection info structure or -1 when not found.
*/
INT32 blecm_FindConMux(UINT16 con_handle);
/**
* Get the GATT DB size given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return GATT DB size or 0 when not found.
*/
UINT16 blecm_GetDbSizeConMux(UINT16 con_handle);
/**
* Get the GATT DB given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return GATT DB or NULL when not found.
*/
void *blecm_GetDbConMux(UINT16 con_handle);
/**
* Get the device information given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return Device information pointer or NULL when not found.
*/
void *blecm_GetDevConMux(UINT16 con_handle);
/**
* Get the SMP information given a connection handle.
* \param con_handle Connection handle of the connection to look up for.
* \return SMP information pointer or NULL when not found.
*/
void *blecm_GetSmpConMux(UINT16 con_handle);
/**
* Reset the connection context.
*/
void blecm_ResetPtrConMux(void);
/**
* Set all the connection contexts to the one for the given connection.
* This is used by the stack to switch connection contexts.
*/
void blecm_SetPtrConMux(UINT16 con_handle);
// Internal function to check if 8-bitor 16-bit length is used in the app's GATT DB.
INT32 blecm_needToGATTDB16( void );
/**
* Enable 16-bit length fields in application GATT DB. This needs to be invoked before the first
* access to GATT DB occurs (early in create function). The GATT DB provided in the set_cfg function
* should use 16-bit lengths.
*/
void blecm_enableGATTDB16( void );
/**
* Disable 16-bit length fields in app GATT DB.
*/
void blecm_disableGATTDB16( void );