- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi ,
I am an absolute newbie in this area(coming from Arduino), and I am trying to do just 1 thing: read value from a temperature sensor and send it to the lightblue app on my iPhone.
I have two questions about this :
1. how do I use the GPIO to read the sensor value?? (or should I use the gpio at all)
Currently, I first added the pins to hello_sensor_gpio_cfg
const BLE_PROFILE_GPIO_CFG hello_sensor_gpio_cfg =
{
/*.gpio_pin =*/
{
GPIO_PIN_WP, // This need to be used to enable/disable NVRAM write protect
GPIO_PIN_BUTTON, // Button GPIO is configured to trigger either direction of interrupt
GPIO_PIN_LED, // LED GPIO, optional to provide visual effects
GPIO_PIN_BATTERY, // Battery monitoring GPIO. When it is lower than particular level, it will give notification to the application
GPIO_PIN_BUZZER, // Buzzer GPIO, optional to provide audio effects
7, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1 // other GPIOs are not used
},
/*.gpio_flag =*/
{
GPIO_SETTINGS_WP,
GPIO_SETTINGS_BUTTON,
GPIO_SETTINGS_LED,
GPIO_SETTINGS_BATTERY,
GPIO_SETTINGS_BUZZER,
1, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0
}
};
Then, in hello_sensor_create(), I added just one line after bleprofile_GPIOInit(bleprofile_gpio_p_cfg);
:
/******* added by ME*/
gpio_configurePin(0, 7, GPIO_INPUT_ENABLE, 1);
And then, in hello_sensor_send_message(),
I used gpio_getPinInput(0,7) to try to read in the sensor's value. However this function returns a BYTE, so I casted it to char and assigned it to the dereferenced pointer *db_pdu.pdu
I don't know what went wrong, but the message does not seem to be sending.
Do you know what I should do with this?? I am just trying to do one simple thing: read a sensor value and send it.
I would appreciate any suggestions from you guys.
Thanks a lot
Solved! Go to Solution.
- Labels:
-
GPIO
-
MasterSlave
-
SDK 2.X
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You should use 0 as gpio_flag. 1 means GPIO_OUTPUT defined in bleprofile.h.
When I read GPIO value as input, I use code like below.
----------
gpio_configurePin(p >> 0x04, p & 0x0f, GPIO_INPUT_ENABLE, GPIO_PIN_OUTPUT_LOW);
...
BLEPROFILE_DB_PDU p_pdu;
p_pdu.len = 0x01;
if (gpio_getPinInput(p >> 0x04, p & 0x0f)) {
p_pdu.pdu[0x00] = 1; // High
} else {
p_pdu.pdu[0x00] = 0; // Low
}
bleprofile_WriteHandle(HANDLE_SAMPLE, &p_pdu);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You should use 0 as gpio_flag. 1 means GPIO_OUTPUT defined in bleprofile.h.
When I read GPIO value as input, I use code like below.
----------
gpio_configurePin(p >> 0x04, p & 0x0f, GPIO_INPUT_ENABLE, GPIO_PIN_OUTPUT_LOW);
...
BLEPROFILE_DB_PDU p_pdu;
p_pdu.len = 0x01;
if (gpio_getPinInput(p >> 0x04, p & 0x0f)) {
p_pdu.pdu[0x00] = 1; // High
} else {
p_pdu.pdu[0x00] = 0; // Low
}
bleprofile_WriteHandle(HANDLE_SAMPLE, &p_pdu);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you very much for the very helpful reply!!!! I shall try it out!!!
Just another quick related questions though:
Is there a way for the tag chip to read analog input instead of digital input??
Thanks a lot!
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
Thank you so much for your reply. I shall look into the analog to digital converter. Thank you so much again.