cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

Anonymous
Not applicable

I tried to modify hello_client and hello_sensor (BCM20737 TAG) to build a piconet:


Master <-> Relay <-> Slave


I use hello_client codes for Master and Relay.  hello_sensor codes for Slave.


I can make it work when there is no bonding/encryption enabled.  However, when I enable the encryption, there is a problem between Master and Relay.


The sniffer shows the following:


Master -> Relay: Pairing Request

Relay -> Master: Pairing Response

Master -> Relay: Pairing Confirmation

Relay -> Master: Pairing Random


then there is no further control messages for encryption.  The link is still there (timeout disabled) but no more control messages.


I can make the Master (hello_client) connects with Slaves (hello_sensor) with encryption.  However, I cannot make the Master (hello_client) connects with Relay (hello_client) with encryption. 


Any idea why is that?  Any difference of the security operations between hello_client (as slave) and hello_sensor?


0 Likes
1 Solution
Anonymous
Not applicable

I still cannot figure out why I cannot use the codes from "hello_client" as a relay with encryption connection. When the encryption is disabled, it can function as a relay.   I later modified the codes of "hello_sensor" to make it as a relay (master/slave) node and it has no problem.

View solution in original post

0 Likes
4 Replies