cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

Anonymous
Not applicable

I tried installing on Win 8.1 and getting the following error for Java runtime machine.

"Could not find a valid Java virtual machine to load

You may need to reinstall a supported Java virtual machine"

Which version of Java VM I need to install?

Thanks in advance.

0 Likes
1 Solution
MichaelF_56
Moderator
Moderator

The WICED SMART SDK utilizes a 32-bit version of an Eclipse based IDE which requires a 32-bit version of JRE to be installed. If you have the 64-bit JRE installed you will need to install the 32-bit version as well. The JRE is designed to allow both 32 and 64 bit variants to be installed on the same system.

View solution in original post

0 Likes
3 Replies
MichaelF_56
Moderator
Moderator

The WICED SMART SDK utilizes a 32-bit version of an Eclipse based IDE which requires a 32-bit version of JRE to be installed. If you have the 64-bit JRE installed you will need to install the 32-bit version as well. The JRE is designed to allow both 32 and 64 bit variants to be installed on the same system.

View solution in original post

0 Likes
MichaelF_56
Moderator
Moderator

Also take a look at Wiced Smart SDK Java issue

j.t

0 Likes
Anonymous
Not applicable

Thanks a lot for quick help. That worked!

Regards,

Satish

0 Likes