cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

MiTo_1583836
Contributor II

Is there any recommendation provided by Broadcom for the SW that should be used to pass the FCC certification for the BCM20736S?


Is there a Test Suite that will be provided by Broadcom that can be used during the FCC certification work? Something that would cover BLE stress test or specific scenarios?



0 Likes
1 Solution
MichaelF_56
Moderator
Moderator

The Manufacturing Bluetooth test tool (MBT) will be introduced in SDK 2.1 and can be used to test and verify the RF performance of the BCM2073x family of SoC Bluetooth Low Energy (BLE) devices.

Each test essentially sends an HCI command to the device and then waits for an HCI Command Complete event from the device.

The following tests will be available using this tool:

  • Reset Test
  • LE Receiver Test
  • LE Transmitter Test
  • LE Test End
  • Continuous Transmit Test

View solution in original post

2 Replies
MichaelF_56
Moderator
Moderator

The Manufacturing Bluetooth test tool (MBT) will be introduced in SDK 2.1 and can be used to test and verify the RF performance of the BCM2073x family of SoC Bluetooth Low Energy (BLE) devices.

Each test essentially sends an HCI command to the device and then waits for an HCI Command Complete event from the device.

The following tests will be available using this tool:

  • Reset Test
  • LE Receiver Test
  • LE Transmitter Test
  • LE Test End
  • Continuous Transmit Test

View solution in original post

MiTo_1583836
Contributor II

Excellent, thanks for listing the detail of the tests.

0 Likes