cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

OrAs_4645701
New Contributor II

Hello

We tried to work with the device CYBT-343026 in HCI mode.

For short period it was working and now we can’t receive any feedback.

We tried to do the hard reset with no success.

We tried to communicate using UART communication which the hex code:

01 03 0c 00.

We tried to rewrite the FW using the Bootloader Host, but we received communication error

When trying to flash the image firmware although the port is connected with baud rate of 115,200

(Screen shot attached)

0 Likes
1 Solution
OrAs_4645701
New Contributor II

Ok guys thanks for the help

It’s look like the chip was gone

We replaced it and disabled the flow control, now it’s works thanks!

View solution in original post

0 Likes
11 Replies
Owen_Zhang123
Moderator
Moderator

Could you take a look at the following blog: Run CYW20706 in HCI Mode

0 Likes
OrAs_4645701
New Contributor II

Hi I tried to work with the issue as it describe in the link.

This time I tried to load an hcd file from:

Documents/WICED-Studio-6.4/20706-A2_Bluetooth/build/hci_audio_remote_control-CYW920706WCDEVAL-rom-ram-Wiced-release/hci_audio_remote_control-CYW920706WCDEVAL-rom-ram-Wiced-release.hcd

Used the WICED Client Control but it’s failed again.

Screen information attached

Thanks

0 Likes
Owen_Zhang123
Moderator
Moderator

There are two HCI mode for the device:

1. standard HCI mode which can accept the HCI command defined in the spec

2. WICED HCI mode which can accept the wiced-defined HCI command. You can refer to the document "WICED-HCI-Control-Protocol.pdf" under the doc folder for details.

If you want to use the standard HCI command:

1. Please download and program the application in the attachment of the blog.Run CYW20706 in HCI Mode

2. Pull CTS to high during the power on reset

3. Use the HCI baudrate defined in the application which is 115200.

Then the device will receive all the HCI command defined in the bluetooth spec.

OrAs_4645701
New Contributor II

I can’t download anything .

Did you see the attachment ?

0 Likes
BoonT_56
Employee

client.jpg

Can you try again? The crucial part is the steps in bringing the board into HCI mode.

0 Likes
OrAs_4645701
New Contributor II

1. I set the CTS to high

2. All the switches set to the direction of the USB connector (For uSB power)

3. I connected the Rx To Tx PC

4. I connected the Tx To Rx PC

5. I connected the ground to ground PC

6. I connected the USB to PC for power.

It’s supposed to start in HCI mode (Because of the CTS high as describe)

I forgot something ?

0 Likes
BoonT_56
Employee

I am using the 343026 EVAL board and so I don't have to do the above.

For the 343026 module, the Recover button actually sets SPI2_MOSI (Pin 9 of the module) to ground for the recovery process.

Can you do the below?

1) Set Pin 9 to ground and hold

2) Reset

3) Release Pin 9 after 1s

4) Do the download again

OrAs_4645701
New Contributor II

If you talking about pin 9 near J7 same problem

I connected Pin 9 to ground and reset the power by unplugging and plugging back the USB

0 Likes
BoonT_56
Employee

I was referring to Pad 9 (SPI2_MOSI) of the physical module (CYBT-343026). This pad has to be brought to GND before resetting.

OrAs_4645701
New Contributor II

As I saw in the scheme it’s the I2C_SDA (E8)

No change

0 Likes
OrAs_4645701
New Contributor II

Ok guys thanks for the help

It’s look like the chip was gone

We replaced it and disabled the flow control, now it’s works thanks!

0 Likes