cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

Anonymous
Not applicable

I purchased BCM92073X_LE_TAG4.  I downloaded the WICED smart SDK and was able to download hello_sensor and communicate with the Windows 10 client example provided in the SDK.  Now I am unable to download anything.  I get the following console output:

20:43:59 **** Build of configuration Release for project WICED-Smart-SDK ****

"C:\\Users\\RothsMark\\Documents\\WICED\\WICED-Smart-SDK-2.2.3\\WICED-Smart-SDK\\make.exe" hello_sensor-BCM920736TAG_Q32 download

Linking target ELF

OK, made elf.

Call to hello_sensor_spar_crt_setup @ 00206195

OK, made C:/Users/RothsMark/Documents/WICED/WICED-Smart-SDK-2.2.3/WICED-Smart-SDK/Wiced-Smart/spar/../../build/hello_sensor-BCM920736TAG_Q32-rom-ram-Wiced-release/A_20736A1-hello_sensor-rom-ram-spar.cgs. MD5 sum is:

1180812d92f07aac93b91d5b37fcf8bd *../../build/hello_sensor-BCM920736TAG_Q32-rom-ram-Wiced-release/A_20736A1-hello_sensor-rom-ram-spar.cgs

--------------------------------------------------------------------------------

Patches start at                  0x00204568 (RAM address)

Patches end at                    0x00205988 (RAM address)

Application starts at             0x00205554 (RAM address)

Application ends at               0x00206191 (RAM address)

Patch size (including reused RAM)       5152 bytes

Patch size                              4076 bytes

Application size                        3133 bytes

                                      ------

Total RAM footprint                     7209 bytes (7.0kiB)

--------------------------------------------------------------------------------

Converting CGS to HEX...

Conversion complete

Creating OTA images...

Conversion complete

OTA image footprint in NV is 9394 bytes

Detecting device...

Device found

Downloading application...

****Download failed - Press the reset button on the device and retry ****

20:44:02 Build Finished (took 3s.137ms)

Pressing what I assume is 'reset', a button labeled 'sw3', has no effect on the problem.

In Windows device mgr I see that connecting the TAG4 board creates 2 COM ports, COM3 and COM4 which are set to 9600 baud.  that seems slow...

Not sure how to debug at this point.  My kit did not contain either a cable or a 'getting started' guide that supposedly come with the board.  But it did work fine but now it fails to download.  If anyone has a soft copy of the 'getting started' guide I would appreciate them sending it to me.

I'm using:

WICED Smart IDE - Eclipse IDE for C/C++ Developers 2.2.3

Version: Juno Service Release 2

Build id: 20130225-0426

0 Likes
1 Solution
Anonymous
Not applicable

huangj, following your note I change my recover command to:

proximity-BCM920737TAG_Q32  download recover UART=COM4

previously I did not have the 'download' parameter.  This worked correctly and the board was recovered.

Thanks!

View solution in original post

0 Likes
5 Replies
BoonT_56
Employee

You may refer to the tag4 board information from the below thread:

Tag 4 Platform Specific Hardware Information

Otherwise, you may have to do a recovery procedure which is detailed in the QSG document.

0 Likes
Anonymous
Not applicable

I found the link last night, but the recovery procedure failed much like the download.

One thing was that the recovery note said to specify 'the' uart. The USB-serial driver creates 2. I tried both but neither recovered the board.

Another thing I found odd: switch 8 was set to the exact opposite of what the startup guide specified.

Mark Roths

Intrinsix

Mobile: (831) 428-1004

0 Likes
Anonymous
Not applicable

Here is the result of my ‘recovery’ attempt:

"C:
Users
RothsMark
Documents
WICED
WICED-Smart-SDK-2.2.3
WICED-Smart-SDK
make.exe" proximity-BCM920736TAG_Q32 recover uart=COM4

Linking target ELF

OK, made elf.

..\..\Tools\ARM_GNU\bin\Win32\arm-none-eabi-objdump: section '.data' mentioned in a -j option, but not found in any input file

Call to proximity_spar_crt_setup @ 002056f9

OK, made C:/Users/RothsMark/Documents/WICED/WICED-Smart-SDK-2.2.3/WICED-Smart-SDK/Wiced-Smart/spar/../../build/proximity-BCM920736TAG_Q32-rom-ram-Wiced-release/A_20736A1-proximity-rom-ram-spar.cgs. MD5 sum is:

50dd86dd78a51c41b7359ce0b69cfa7c *../../build/proximity-BCM920736TAG_Q32-rom-ram-Wiced-release/A_20736A1-proximity-rom-ram-spar.cgs

0 Likes
huangj
Contributor

Hi mroths,

There is a download log in the folder(WICED-Smart-SDK-2.X.X\WICED-Smart-SDK\build\your app name\download. You can see the reason.

You also can add some parameter in your make target.

For example:

hello_sensor-BCM920736TAG_Q32 download BT_DEVICE_ADDRESS=1234567890CD UART=COM7

or

proximity-BCM920737TAG_Q32  download recover UART=COM13

Here is the my successful recovery message:

--------------------------------------------------------------------------------

10:29:01 **** Build of configuration Release for project WICED-Smart-SDK ****

"C:\\Users\\Jack\\Documents\\WICED\\WICED-Smart-SDK-2.2.2\\WICED-Smart-SDK\\make.exe" proximity-BCM920737TAG_Q32 download recover UART=COM13

Linking target ELF

OK, made elf.

..\..\Tools\ARM_GNU\bin\Win32\arm-none-eabi-objdump: section '.data' mentioned in a -j option, but not found in any input file

Call to proximity_spar_crt_setup @ 00205445

OK, made C:/Users/Jack/Documents/WICED/WICED-Smart-SDK-2.2.2/WICED-Smart-SDK/Wiced-Smart/spar/../../build/proximity-BCM920737TAG_Q32-rom-ram-Wiced-release/A_20737A1-proximity-rom-ram-spar.cgs. MD5 sum is:

f0f524a9a2d66f8cede34c18b1cd8c90 *../../build/proximity-BCM920737TAG_Q32-rom-ram-Wiced-release/A_20737A1-proximity-rom-ram-spar.cgs

Patches start at                  0x00204568 (RAM address)

Patches end at                    0x002056B0 (RAM address)

Application starts at             0x002052A0 (RAM address)

Application ends at               0x00205444 (RAM address)

Patch size (including reused RAM)       4424 bytes

Patch size                              3384 bytes

Application size                         420 bytes

                                      ------

Total RAM footprint                     3804 bytes (3.7kiB)

--------------------------------------------------------------------------------

Converting CGS to HEX...

Conversion complete

Creating OTA images...

Conversion complete

OTA image footprint in NV is 5983 bytes

Downloading application...

****Download failed - Press the reset button on the device and retry ****

Recovering platform ...

Recovery complete

Application running

10:29:13 Build Finished (took 12s.163ms)

Jack

Anonymous
Not applicable

huangj, following your note I change my recover command to:

proximity-BCM920737TAG_Q32  download recover UART=COM4

previously I did not have the 'download' parameter.  This worked correctly and the board was recovered.

Thanks!

View solution in original post

0 Likes