cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

Anonymous
Not applicable

The BCM20737 datasheet (Document 20737-DS100-R) states (on page 13) that the BCM20737 provides mechanisms for implementing security and authentication schemes, and that the details on how to use this functionality "are available in application notes in this topic."

Do these application notes exist ?  If yes, where can I get them ?

0 Likes
1 Solution
2 Replies
MichaelF_56
Moderator
Moderator

Correct.  I believe this is referencing the RSA functionality available through the Polar SSL library that is included in ROM within the 20737.

The link boont references is the only documentation we can provide for this functionality currently.

However, I wanted to also note that the secure OTA sample app uses the RSA functionality as well, so perhaps you could reference it as well.

0 Likes