Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

LVTTL is a JEDEC standard that references the input signal to ground. The output switching range is 0.4 to 2.4V for 3.3V LVTTL and 0.4 to 2.2V for 2.5V LVTTL .

   

HSTL is a technology-independent interface standard for digital ICs that calibrates the input signal to a reference voltage rather than to ground. This calibration enables a smaller I/O swing and improves performance. HSTL was developed for voltage-scalable and technology-independent I/O structures. The nominal logic-switching range is 0.65 to 0.85V for 1.5V HSTL, resulting in faster outputs with reduced power-dissipation and signal-integrity issues.

   

 

   

For more details refer to the article below:

   

http://www.edn.com/article/476349-Exploring_memory_interface_options.php

0 Likes
1 Reply
Anonymous
Not applicable

QDRII/II+ SRAMs adhere to the HSTL I/O standard.

   

Sync/NOBL SRAMs adhere to the LVTTL I/O standard.

0 Likes