S6AE101A avoid storage capacitor and changing power in options

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
rapo_4657801
Level 1
Level 1

Hello,

We intended to use S6AE101A in one of Design.

We would like to modify input options

VBAT will be supplied with 5V DC

VDD will be supplied with 2 to 3V from Coin cell battery.

expected output is 3V.@100mA

will this modification in input supply affect ?

Is there any way we can avoid storage cap?

Thanks,

Raghu

0 Likes
1 Solution
EijiF_46
Employee
Employee
10 likes received First like received

Hi Raghu

We recommend to use S6AE102A device for the input options. In case of using S6AE102A, please connect as the following:

- VDD will be supplied with 5V DC with protection series resister (around 50-OHM).

- VBAT will be supplied with 2 to 3V from Coin cell battery.

Thanks

View solution in original post

0 Likes
1 Reply
EijiF_46
Employee
Employee
10 likes received First like received

Hi Raghu

We recommend to use S6AE102A device for the input options. In case of using S6AE102A, please connect as the following:

- VDD will be supplied with 5V DC with protection series resister (around 50-OHM).

- VBAT will be supplied with 2 to 3V from Coin cell battery.

Thanks

0 Likes