Power MOSFET

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
ambition
Power MOSFET
兄弟们,我想利用数学模型计算SIC MOSFET的损耗,自己推导公式如下,计算结果与datasheet的Eon结果偏差太大,看论文中考虑了寄生电容的非线性,采用了了分阶段恒定电容模型,猜测是这个导致的偏差,我用的管子FF6MR12W2M1P_B11   Show More
ambition
Power MOSFET
The loss of loss obtained by the MOSFET loss calculation based on the MOSFET loss is far from the IPOSIM simulation, as follows is the loss calculatio... Show More
ambition
Power MOSFET
根据自己推导的 mosfet损耗计算式计算得到的损耗与IPOSIM仿真得到的相差很远,如下是BOOST电路下管的损耗计算,麻烦哪位能告知哪里有问题。或者哪位有比较好的计算损耗的资料,网上的论文好多都是根据Qgd,Qgs计算,但英飞凌的芯片手册并不提供这些。   Show More
Hasan2021
Power MOSFET
Hi there,I am looking for a customized design where good power solution can be applicable.My aim is to develop a DC-DC sutable toloplogy ( flyback, bu... Show More
Anonymous
Power MOSFET
Hello,I am looking for the parameter Rθ(JB) (Thermal resistance Junction - Board) for MOSFET item No. IPT65R033G7XTMA1. Is this information available ... Show More
cicien
Power MOSFET
Hello, I have a question about MOSFET. How to test the FET SOA? Is the SOA in the data manual a trend chart? If the DC test method is adopted, what s... Show More
fionut
Power MOSFET
Hello I know I have posted in the wrong section, but I could not find any section dedicated to SMPS controllers , under power category.   IDP2303A PFC... Show More
Harold
Power MOSFET
I want to use a MOSFET as a switch driven by my microcomputer.     The original circuit using N-channel MOSFET is on the left side. Honestly, I do no... Show More
MS_19060803
Power MOSFET
いつもお世話になっております。 パッケージ(PG-HSOF-8)の内部構造についてご教示いただけないでしょうか。   下記のANのP.5にパッケージ内部が記載されています。 ↓ https://www.infineon.com/dgdl/Infineon-ApplicationNote_650V_CoolMOS_C7_Gold_TOLeadless.pdf-AN-v01_01-EN.pdf?fileId=5546d46253f65057015495adbf15197d... Show More
MS_19060803
Power MOSFET
いつもお世話になっております。 パッケージ(PG-HSOF-8)のパワーサイクル試験のデータ要求がございましので データを取得されていましたら、情報を開示して頂けないでしょうか?   デバイスはIPT030N12N3 Gになります。   また、パッケージ(PG-HSOF-8)よりパワーサイクルの長い... Show More
Board Information

Power MOSFET

In this forum you can post your questions, comments and feedback regarding Power MOSFETs. Infineon offers a wide range of Power MOSFET families for low and high power applications with voltages ranging from -250V to 1700V. The Low an Medium voltage families feature the OptiMOS™ and StrongIRFET™ power MOSFET families. The high voltage MOSFETs feature CoolMOS™ MOSFET technology.
Top liked authors