Power MOSFET

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
SoU_4942226
Power MOSFET
いつもお世話になっております。 MOSFETのリード製品の温度測定ポイントをご教示いただけないでしょうか。 下記のANのP.4に記載の内容から裏面の中央が測定位置になると考えていますが認識間違いないでしょうか。 https://www.infineon.com/dgdl/Infineon-Recommendations_for_Board_Assembly_TO-AP-v02_00-EN.pdf?fileId=db3a3043183a955501189e662ae34052... Show More
DJTao
Power MOSFET
  What does each character mean for the six characters on the body? eg. GAT036 on attached picture. Thanks in advance for help   Show More
Harold
Power MOSFET
I'm not sure if I can drive a 24V (0.5A) dc motor with the following circuits?I fear that there will be burned too much power in the transistor when t... Show More
User19686
Power MOSFET
Hello,The package of this component is PG-TDSON-8-33. The Rthja is 50K/W with a 6 cm² cooling area on a one layer 70µm copper PCB.Does anyone know the... Show More
树暖
Power MOSFET
选用BAR6402VH6327XTSA1型号的二极管进行整流电路测试时,发现在幅值为2V的正弦输入下,输出波形幅值随频率增大而逐步减小。但根绝数据手册显示,该二极管的频率范围应为1MHz~6GHz,所用频率未超过,不清楚问题所在? 电路图: 1MHz时波形:(绿:Vi;黄:Vo 10MHz时波形... Show More
SoU_4942226
Power MOSFET
いつもお世話になっております。TO-220 FullPAK Narrow Leads の実装方法についてご相談させてください。端子の根元部分まで基板穴に挿入して、部品パッケージを基板上に載せた状態(以下の図)で、基板に実装、使用しても問題ないでしょうか? 下記の実装に関するアプリケーションではリード... Show More
SoU_4942226
Power MOSFET
いつもお世話になっております。Super SO8 (PG-TSON-8-3) 実装のパターンについてご相談させてください。Packageのページより抜粋しております。https://www.infineon.com/cms/en/product/packages/PG-TSON/PG-TSON-8-3/... Show More
User17437
Power MOSFET
Hey GuysI have this strange problem with all IRPS5401 on our new PC Board. Even though the devices are configured properly, they won't start-up the ou... Show More
User22701
Power MOSFET
Hello all,I am using OrCAD Pspice to run a simulation and I want to include the model for IPD90N08S4-05 (in reality it is AUIRFR3607, but it is marked... Show More
User22659
Power MOSFET
Hi,I was wondering about kelvin-source mosfets. Is kelvin-source pin and the power source pin have mechanical connection or they isolated?What happene... Show More