cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable
        Hi,   
   
I am working on cy3214 PSOC eval usb evalution board. I have installed Psoc designer 4.3v. This board uses cy8c24794 IC. I am trying to download a project which is got by installing the designer using Psoc programmer. It is showing that it is connected but when clicked on program it will show busy and fail. it is not getting programmed. so i want a example project built with cy8c24x94 device family and cy8c24794 device.   
   
Thanks and regards   
0 Likes
1 Reply
pushekm_21
Employee
        Hi,   
   
First of all I would like to suggest you is Upgrading the designer version. This is very very old version of PSoC Designer. The current version of PSoC Designer is PD5.0 SP4 and PSoC Programmer is v3.05.   
   
The dummy project attached might help.   
   
Regards   
Pushek   
0 Likes