example bootloadable blinkLED throws exception when loaded

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Opening a workspace with bootloader example(bootloadable blinkLED.cyprj with SCB_bootloader.cywrk), Creator returns with exception ’System.NullReferenceException’.
When 'contiue' clicked, a window opens with 'Reload Modified files ?'
All other projects/examples tested were loading properly.

file: CY8CKIT-049-41xx Example Projects.zip
PSoC Programmer 3.20.0, PSoC Creator 3.0 Component Pack 7, USB-Serial driver 3.13.0.21
WinXP SP3, 2GB RAM, >10GB Disk

   

 

   

Any hints ?

   

 

     
0 Likes
1 Solution
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Could it be that you need to build the bootloader project first, with the same version of Creator you are using for the Bootloadable project?

View solution in original post

0 Likes
5 Replies
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Could it be that you need to build the bootloader project first, with the same version of Creator you are using for the Bootloadable project?

0 Likes
Anonymous
Not applicable

hmm, good point.

   

But the example was packaged with

   

       CY8CKIT-049-41xx Example Projects.zip.

   

Same page referenced to the actual Creator 3.020.

0 Likes
Anonymous
Not applicable

If bootloadable blinking LED.cyprj is loaded instead of .cywrk, .NET issues the exception instead.

0 Likes
Anonymous
Not applicable

After uninstalling and re-installing PSoC  the example bootloader pgm loads and builts like charm.

   

.-)

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Congratulations!

   

 

   

Bob

0 Likes