cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

problem 1

   

i am using the 8c29466 in a sensor application mounted on the shaft of a generator in a power plant.

   

i am using the atraflex awp24s module

   

i wanted to use the cyfispi module, but only the cyfisnp shows up in the rf user modules.

   

the files for the cyfispi are in the following directory

   

C:\Program Files\Cypress\PSoC Designer\5.1\Common\CypressSemiDeviceEditor\Data\SHAREDUM\CYFISPI

   

how can i accomplish this?

   

problem 2

   

i would use the snp but i can not find a sniffer to test if the packets are being generated

   

artaflex has the awp24u which works with the cyfispi (fixed channel, freq, ect...)

   

is there a usb hub with sniffer app that will work with the cyfisnp?

   

 

   

appreciate any help

0 Likes
1 Reply
Anonymous
Not applicable

 I need this user module too. We are going to conduct some radio certification tests in a week and I was just informed that some of the tests need a higher level of control that I can't achieve with CyFiSNP. Please help with a hot fix to be able to add CyFiSPI!

   

 

   

Best Regards

   

 

   

/Marcus Hamberg

0 Likes