cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

Hello everyone,

   

I wish to build a battery charger where I can cotrol the output voltage & current to give a total of 300VA.

   

In that I want-

   

1. Current control &

   

2. Voltage control

   

totalling to 300VA.

   

         While charging the battery I want <=85% charging should be a boost charging (rapid charging with high current) & the next 15% should be a trikle charging (continuous charging with low current).

   

         Also I want the feature of Auto turn-off at full charge & setting a minimum limit to start the charging.

   

Please guide me on this.

   

Thanks & Regards-

   

Amit

0 Likes
2 Replies
Anonymous
Not applicable

 Amit,

   

I believe the following Application Note would be a good starter:

   

AN73468 - PSoC® 3 and PSoC 5LP - Single-Cell Lithium-Ion (Li-ion) Battery Charger

   

Link: http://www.cypress.com/?rID=58095

   

Regards

   

PSoC Wonders!

0 Likes
Anonymous
Not applicable

Hello sir, thanks for considering. I will definitely go through the suggestions &  see how much would it help.

   

Regards-

   

Amit

0 Likes