PSoC™ Creator & Designer Forum Discussions
Dear SIr/madam,
doubts regards program loading using JTAG Protocol.
using PsoC5LP family mc CY8C5868AXP-035 , program through miniprog4. but in miniprog4 we cant choose JTAG protocol, default SWD protocol only coming. by using the setup, i want to load .hex file using JTAG protocol. give some suggestions.
Show LessI got this after updating a project to the latest PSoC Creator.
It is caused by Application.cyprj containing two entries with different capitalization of the names ("PSoC" vs "PSOC"), and it can't fix the capitalization difference. Manually editing the cyprj file to make them consistent fixes it, or deleting the folder from Generated Source PSoC3 and letting it regenerate.
Hello,
I am working on Legacy Code of the organization.
Code was compiled using : PSoC Creator 1.0 Service Pack 2. For some important tasks in the organisation I need to re-compile the code using the same IDE version. Though I searched your website, didn't get this IDE version even in Archive.
Please do help me here at your earliest
Show LessHi all,
I've got a fairly minor issue with PSoC Creator 4.1.
I have a project information text (.txt) file I use to keep a text change log for projects. I normally code in a "dark" theme as I find it easier on the eyes. I'd like to have the text editor in Creator do have the same color scheme (or at the very least just a dark background with white text).
I go to the Tools>Options>Text Editor>Fonts and Colors menu and select "Other" for the file type. I choose a different background color, a dark grey, and this works fine when I hit apply. However it looks like adjusting Item Foreground color does not have any effect when hitting Apply, and even restarting Creator after changing the setting doesn't apply it. See the attached screen capture, you can see the text color does not match the settings:
Is this a known issue? Something wrong only with my setup? Fixed in 4.2?
Any thoughts are appreciated.
Thanks!
Show LessHi,
May I know where can I download PSOC Creator 1.0 Service Pack 2 and PSOC Creator 2.0 Component Pack 3?
Our customers are uisng old PSOC Creator, when we try to migrate the firmware to PSOC 3.0 and above, the program is not working. We would like to have the old PSOC creator software for the fiemware modification.
Thanks,
Jason
Show LessHello everyone,
I have a question regarding the heart sensor. I saw this topic on the internet:
I took thist project:
and saw the following code:
- First, I didn't understand what this interruption does.
- Second, in the part "bpm = 60000 / beat;", I understood that it would be how many pulses he gave 60000 milliseconds divided by the amount of pulses he gave in that time, however in the part "beat = ADC_GetResult16 (0);" does it take the amount of pulses in 60000 milliseconds? I didn't get it right.
I am having trouble figuring out why these errors are occurring. I looked at my .h file and I only have macros defined so I don't know where the issue is occurring. Also, I am having trouble with trying to figure out the 'arm-none-eabi.exe' failed error.
Show LessHi,
Is there any way to generate doxygen documentation inside a PSoC Creator Project without leaving the PSoC Creator? That means without calling manually doxygen in a terminal or using Doxywizard.
Regards.
Show LessI have this programmer.
I am trying to detect the board with
https://www.cypress.com/documentation/software-and-drivers/cypress-programmer-archive
this software but it can not detect.
Do anything extra i need to download or update to be able to program the MCU alongside with this board with this sofware.
Show Less