PSoC™ Creator & Designer Forum Discussions
I have imported "Thermistor_Calc" to PSoC Creator CyComponentLibary.cyprj from "AN66477-PSoC35 Temperature Measurement with Thermistor" .
Then I created my project and add the Thermistor_Calc component. But there always has error while I built my project. See below screenshots. And it is surprising that no any error notice while I built the origin AN66477 project. And the config window is differenct between them.
Also, there is no Component Preview in Component Catalog. Seems it has not been imported successful. But I do not know why. Anyone can help?
Show LessAre there times when your development PC can't be connected to the internet? To ensure that you always have the latest version of Cypress software, please navigate to www.cypress.com, mouse-over "MyAccount" and click on MySubscriptions. From there you can select the PSoC Designer CD subscription and then click save. Every time a new version of PSoC Designer is released, we'll automatically send you the software on CD - nothing more you need to do!
Note that you'll need to be a registered cypress.com user with a mailing address on file.
PSoC Designer 5.1 SP2 and PSoC Programmer 3.13 are now released through CyInstaller and website www.cypress.com/go/psocdesigner.
The PSoC Designer 5.1 SP2 release has added the notable features:
• SmartSense_EMC User Module Support for CY8C20xx6AS devices.
• Ovation ONS II LP, LPNAV User Module support for CYONSFN3050 devices.
• Expanded LINS User Module Support to CY8C29xxx Devices.
• Support for the CyInstaller v2.1
• PSoC Designer Live Landing Page
• Numerous defect fixes
• Ease of Use Improvements
PSoC Programmer 3.13 release has added the notable featuers:
• Patch programming support for FX2 based programmers (example, FTK3/5)
• Improve JTAG programming algorithms
• Update to the Miniprog3 firmware
• Touch Tuning Bridge Firmware update
• Support for Bridge Control Panel v1.3 which adds bar graph charting capabilities
• New Device support which includes numerous new Touch devices.
The existing library of communications components seems to have most of the bases covered.
One thing I could use that isn't there is a 1-wire component.
It's possible to make one out of a UART with some wacky wiring (wire the rx and tx pins to the input and output sides of a pin in resistive pull up mode), some ISRs, and a small API but it would be nice to have a tested and validated one that everyone could use.
Show LessThere will be a free webinar tomorrow on creating a Bootloader in PSoC. You can get it's WebEx information, and see all upcoming live webinars here: http://www.cypress.com/?rID=51939
Hope you can make it!
-Bobby
Show LessI have a PSoC3 Project. I want to know the version of Creator on which it was built last time.
How do I take signals from one schematic page to another? I know I can make the sheet larger, but I see the symbol for an connector, so I'm wondering how to use it.
Shawn
Show LessThe Keil documentation includes a
#pragma small
directive to allow small model code to be generated on a function or file scope. If I put the directive in the file I get the following error:
ERROR: :#pragma SMALL: PARSING INVOKE-/#PRAGMA-LINE RESPECIFIED OR CONFLICTING CONTROL
since the PSoC Creator command line has the LARGE directive. Is there any way to remove the LARGE directive from the command line?
Show LessIf I rename or remove some components, I get a new copy of the generated source with the correct name, which is good. I also get the new source added to the project and the old source removed.
Less good is that even the "Clean and build" option doesn't remove the old generated source from disk.
Show LessI got an illegal macro name in PSoCGPIOINT.h Generated by PSoC Designer 5.1.2101.0
As this file is generated by Designer, I can't modify it, it is rewritten on every build.
I use standard Imagecraft compiler.
Any Idea to fix this ?
Thanks
Show Less