PSoC™ Creator & Designer Forum Discussions
I create a design project. I create two library projects. I declare that the design project has code dependencies on both of the library projects.
I build everything.
The link step fails because only one of the libxxx.a or libyyy.a files (generated by building the library projects) is added to the linker command line. I can control which one is added to the linker line by the order in which I add the dependencies (not the order in which they are listed). It appears that the first dependency that is added is respected and the second one is ignored.
Is this a known bug/restriction?
Any thoughts on work arounds? (besides jamming the two libraries together into one library project and messing up my nice factoring)
Thanks.
Show LessHi,
I am trying to set up a 4-channel communication link between Xilinx Kinetix-7 SerDes as Receiver and Cypress CYP15G0401DXB hotlink II chip as transmitter, the protocol to support is Fibre Channel 1994, but I am having issues on channel bonding and clock correction. It seems that CYP15G0401DXB uses a special 16 word Sync Sequence for channel bonding which doesn't work on Xilinx SerDes Receiver and Xilinx Receiver requires some special characters for clock correction, which the Cypress transmitter couldn't provide in the Fibre channel protocol.
would it be easier for me just to implement clock correction and channel bonding logic by myself in FPGA?
Does anyone have similar exprience and could you share some information on how you solved the issue?
Thanks.
Jason
Show LessHi,
For my recent project I needed to use three different I2C buses, unfortunately I'm using PSoC5,
and apparently as for now you can't use more than two I2C modules for PSoC5 nor three
I2C modules for PSoC3.
So, with some help of the support team and a couple hours of work and experiments
I mannaged to desgin a component which uses only one built in I2C module which let you
mux four different I2C buses. I found it very usefull. The drawback of this method is of course the speed
limit of 100kbps.
I also made a simple I2C driver for this module and tested the component.
Is someone interested?
Show LessI am new to Cypress. I wanted to start develop with PSoC4. I have donwnloaded the PSoC creator 3.3. whenever I open the project file it shows the message as
Unable to open the workspace
"D:\R&D_Progress\touch\PSoC\exapmles\LAB2PSoC 4 Intro Lab Solutions.cywrk.Archive01\Lab Solutions\PSoC 4 Intro Lab Solutions.cywrk": (Invalid character(s): &). Address the error and try again.
Show LessHello,
when developing a project in PSoC Creator, doesn't matter which one, It's common that we may have to choose the pins and ports. I know that depending on the component the PSoC Creator automatically assign a pin, for example the UART component has pre-defined Rx/Tx pins. But if I want to use a PGA, ADC, and others components, can I choose any pin that I want? Or should I only use the pins that hasn't anything pre-established (like OpAmp[1].vminus, or XTal.Xo, or any other)?
Show LessIn PSOC Creator, is it possible to have multiple projects that share a "top design". For example, you come up with a "hardware" design -- schematics, pin assignments, clocks, etc. You want to use this same design in two projects -- same "hardware", same generated software but with different user specified software, for example, a different main, etc.
Clearly, you can just copy a project and get two projects with the same design but this gives you two separate designs to maintain.
Any ideas?
Thanks.
Show LessHello.
This is funny, I am writing about automatic pin assignments and another developer is asking about manual pin assignments.
In one of the videos from Cypress I thought I caught something about allowing PSoC Creator to automatically select pin assignments because it will pick the pins best suited for optimum performance.
I do not recall the video or how to get back to it. But even more importantly, if this is correct, how do I instruct PSoC Creator to "auto-route" the pins?
And as the other post mentions I am not talking about specific functions but things such a LCDs, Push-Buttons, LEDs, etc.
Thank You,
Doug
Show LessDear Sirs,
My company is going to upgrade Window OS from 7 to 10. What I have developed the PSoC USB interface works on Window 7 64-bit OS is OK. Does USB diver -- cyusb.sys works on Window 10 OS?
If not, where can download latest version of cyusb.sys and cyusb.inf?
Regards
Qingshan
Show LessA faster not completely accurate version for multiplying two single numbers:
I've written a very fast floating point multiplier for another project that may be able to significantly speed up 3d printer software. This routine hacks the internal format of normalized IEEE 754 single precision floating point numbers.
As most of you probably know, you can take a fixed point integer, and shift left << 1 to multiply by 2, or shift right >> 1 to divide by 2.
This technique will break down one of the multiplacants bit by bit, and add the other to itself using a fixed point addition to perform the multiplication. For example, ff you want to multiple x by 5, that is the same as 4*x + 1*x; 4*x is x << 2.
DISCLAIMER: This is a hack... it is not completely accurate (only 5 decimal digits or so). It does not work with denormalized numbers, the numbers smaller than 1 e -38 or so and does not currently track, respect or report underflow, overflow, nan or infinity.
float fFastMult(float f, float g) {
uint32 *pf = (uint32*) &f;
uint32 *pg = (uint32*) &g;
uint32 ufExp = *pf & SINGLEEXPBITS;
if (!ufExp) return(0); // Not competely accurate for denormalized numbers
// if (ufExp == SINGLEEXPBITS) { ... // Detect and handle inf, nan, etc.
uint32 ugExp = *pg & SINGLEEXPBITS;
if (!ugExp) return(0); // Not completely accurate
for denormalized numbers
uint32 uSign = *pf ^ *pg;
uSign &= 0x80000000;
*pf &= SINGLEMANTISSABITS; // Get only mantissa
*pf |= SINGLELEADINGBIT; // Set top assumed bit of Mantissa
uint32 uBits = *pf;
*pg &= 0x7FFFFF; // Note, we will be adding to f, so we automatically get the first assigned bit for free.
while (*pg & 0x00ffffff) {
if (*pg & 0x00800000) { // Note, never true for first time through the loop since we didn't set the assumed ugMantissa bit.
*pf += uBits;
}
*pg <<= 1;
uBits >>= 1;
}
while (*pf & 0xFF000000) {
*pf >>= 1;
ufExp += FASTDOUBLE;
}
ufExp += ugExp - 0x3F800000;
//if (ufExp & 0x807FFFFF) {... // A chance to test for overflow errors.
*pf &= 0x007FFFFF; // Clear the assumed top bit of the mantissa
*pf |= ufExp | uSign; // And we have our answer... sign, exponent, mantissa
return(*pf);
}
Please note... additional speed gains can be made by rewriting this code specifically for an 8-bit processor. For example:
while (*pg & 0x00ffffff) {
...
*pg <<= 1;
}
can be rewritten:
while (*pg.LSB & 0xff) {
if (*pg.BYTE3 & 0x80) {
...
*pg <<= 1; // Long shift
}
<byte shift down *pg to *p16g, a uint16 rather than a uint32>
while (*p16g.LSB & 0xff) {
if (*p16g.BYTE2 & 0x80) {
...
*p16g <<= 1; // word shift
}
<byte shift down *p16g to *p8g, a uint8 rather than a uint16>
while (*p8g & 0xff) {
if (*p8g & 0x80) {
...
*p8g <<= 1; // Byte shift
}
Note... it is best that the 2nd parameter, g, is a simple number. For example, fFastMult(2.33, 2.0) is much faster than fFastMult(2.0, 2.33).
----
And a version that uses a 16bit x 16bit hardware multiply if it is available:
#define FASTDOUBLE 0x00800000
#define FASTMULT4 0x01000000
#define FASTHALF 0xff8000000
#define FASTDIV4 0xff000000 // Note the signed
#define SINGLESIGNBIT 0x80000000
#define SINGLEEXPBITS 0x7f800000
#define SINGLEMANTISSABITS 0x007fffff
#define SINGLELEADINGBIT 0x00800000
// Currently Set for Little Endian
typedef union {
float f;
uint32 u;
int32 i;
struct {
uint16 LSW;
uint16 MSW;
} w __attribute__ ((packed));
struct {
uint16 LSW;
uint16 MSW;
} ws __attribute__ ((packed));
struct {
uint8 LSB;
uint8 LSBH;
uint8 MSBL;
uint8 MSB;
} b;
struct {
int8 LSB;
int8 LSBH;
int8 MSBL;
int8 MSB;
} c;
} floatint; // __attribute__ ((packed));
float fFastMult(float f, float g) {
floatint *pf = (floatint *) &f;
floatint *pg = (floatint *) &g;
uint32 uTemp = SINGLEEXPBITS; // Intended to be loaded
into a register for fast use.
uint32 ufExp = (*pf).u & uTemp; // SINGLEEXPBITS;
if (!ufExp) return(0); // Denormalized numbers
==> 0
// if (ufExp == SINGLEEXPBITS) { ... // Detect and handle
inf, nan, etc.
uint32 ugExp = (*pg).u & uTemp; //SINGLEEXPBITS;
if (!ugExp) return(0); // Denormalized numbers
==> 0
uTemp = FASTDOUBLE;
ufExp += ugExp - 0x3f800000;
ufExp |= (((*pf).u ^ (*pg).u) & 0x80000000); // uSign = *pf ^
*pg
(*pg).u &= SINGLEMANTISSABITS; // Note, we will be adding
to f, so we automatically get the first assigned bit for free.
(*pg).u |= SINGLELEADINGBIT; // Set top assumed bit of
Mantissa
(*pf).u &= SINGLEMANTISSABITS; // Get only mantissa
(*pf).u |= SINGLELEADINGBIT; // Set top assumed bit of
Mantissa
// This is the full multibyte multiply.
//uint32 uLowByteMult = (*pf).b.LSB * (*pg).b.LSB;
//uLowByteMult >>= 8;
//uLowByteMult += (((*pf).b.LSBH * (*pg).b.LSB) + ((*pf).b.LSB *
(*pg).b.LSBH));
//uLowByteMult >>= 8; // Only the *CARRY* bit
matters... We're skipping it!
//uLowByteMult += (((*pf).b.MSBL * (*pg).b.LSB) + ((*pf).b.LSB *
(*pg).b.MSBL));
uint32 uLowByteMult = (((*pf).b.MSBL * (*pg).b.LSB) + ((*pf).b.LSB
* (*pg).b.MSBL));
(*pg).u >>= 8;
(*pf).u >>= 8;
// Note, it is possible here to detect if the 2nd bit of both *pf and *pg are set.
// in this case, 2 overflow bits are guaranteed allowing the following to work:
// *pf or *pg >> 7, the other >> 8;
// *pf *= *pg; // The assumed mantissa bit overflows, negating the need for an & (bitwise and) operation
// Mantissa (without the LEADING BIT) = *pf >> 9
// Requires an additional *ufExp += FASTDOUBLE;
// Could do this as a long long (32 x 32 => 64 bit) multiply, but this is MUCH faster for on hardware that
// supports 16b x 16b multiply
(*pf).u *= (*pg).u;
(*pf).u += uLowByteMult;
// Note... Top two bits are overflow.
// We need to check them, and shift the
if ((*pf).u & 0x80000000) { // Check for overflow.
ufExp += uTemp; // FASTDOUBLE;
(*pf).u >>= 1;
}
(*pf).u <<= 2; // Shift result to remove top bits (Same as & 0x7fff...)
(*pf).u >>= 9;
(*pf).u |= ufExp; // And we have our answer...
sign, exponent, mantissa
return((*pf).f);
}